ACMP_Init_TypeDef Struct ReferenceEMLIB > ACMP
ACMP initialization structure.
Definition at line
636
of file
em_acmp.h
.
#include <
em_acmp.h
>
Data Fields |
|
uint32_t | biasProg |
bool | enable |
bool | fullBias |
bool | halfBias |
ACMP_HysteresisLevel_TypeDef | hysteresisLevel |
bool | inactiveValue |
bool | interruptOnFallingEdge |
bool | interruptOnRisingEdge |
bool | lowPowerReferenceEnabled |
uint32_t | vddLevel |
ACMP_WarmTime_TypeDef | warmTime |
Field Documentation
uint32_t ACMP_Init_TypeDef::biasProg |
Bias current. See the ACMP chapter about bias and response time in the reference manual for details. Valid values are in the range 0-7.
Definition at line
649
of file
em_acmp.h
.
Referenced by ACMP_Init() .
bool ACMP_Init_TypeDef::enable |
If true, ACMP is being enabled after configuration.
Definition at line
714
of file
em_acmp.h
.
Referenced by ACMP_Init() .
bool ACMP_Init_TypeDef::fullBias |
Full bias current. See the ACMP chapter about bias and response time in the reference manual for details.
Definition at line
639
of file
em_acmp.h
.
Referenced by ACMP_Init() .
bool ACMP_Init_TypeDef::halfBias |
Half bias current. See the ACMP chapter about bias and response time in the reference manual for details.
Definition at line
644
of file
em_acmp.h
.
Referenced by ACMP_Init() .
ACMP_HysteresisLevel_TypeDef ACMP_Init_TypeDef::hysteresisLevel |
bool ACMP_Init_TypeDef::inactiveValue |
Inactive value emitted by the ACMP during warmup
Definition at line
699
of file
em_acmp.h
.
Referenced by ACMP_Init() .
bool ACMP_Init_TypeDef::interruptOnFallingEdge |
Enable setting the interrupt flag on falling edge
Definition at line
652
of file
em_acmp.h
.
Referenced by ACMP_Init() .
bool ACMP_Init_TypeDef::interruptOnRisingEdge |
Enable setting the interrupt flag on rising edge
Definition at line
655
of file
em_acmp.h
.
Referenced by ACMP_Init() .
bool ACMP_Init_TypeDef::lowPowerReferenceEnabled |
Low power reference enabled. This setting, if enabled, reduces the power used by the VDD and bandgap references.
Definition at line
704
of file
em_acmp.h
.
Referenced by ACMP_Init() .
uint32_t ACMP_Init_TypeDef::vddLevel |
Vdd reference value. VDD_SCALED = VDD * VDDLEVEL * 50mV/3.8V. Valid values are in the range 0-63.
Definition at line
710
of file
em_acmp.h
.
Referenced by ACMP_Init() .
ACMP_WarmTime_TypeDef ACMP_Init_TypeDef::warmTime |
Warmup time. This is measured in HFPERCLK cycles and should be about 10us in wall clock time.
Definition at line
678
of file
em_acmp.h
.
Referenced by ACMP_Init() .
The documentation for this struct was generated from the following file:
-
C:/repos/embsw_super_h1/platform/emlib/inc/
em_acmp.h