TIMER_CC_TypeDef Struct ReferenceDevices

TIMER_CC EFM32WG TIMER CC.

Definition at line 46 of file efm32wg_timer_cc.h .

#include < efm32wg_timer_cc.h >

Data Fields

__IOM uint32_t CCV
__IOM uint32_t CCVB
__IM uint32_t CCVP
__IOM uint32_t CTRL

Field Documentation

__IOM uint32_t TIMER_CC_TypeDef::CCV

CC Channel Value Register

Definition at line 48 of file efm32wg_timer_cc.h .

Referenced by TIMER_CaptureGet() , TIMER_CompareSet() , and TIMER_Reset() .

__IOM uint32_t TIMER_CC_TypeDef::CCVB

CC Channel Buffer Register

Definition at line 50 of file efm32wg_timer_cc.h .

Referenced by TIMER_CompareBufSet() , and TIMER_Reset() .

__IM uint32_t TIMER_CC_TypeDef::CCVP

CC Channel Value Peek Register

Definition at line 49 of file efm32wg_timer_cc.h .

__IOM uint32_t TIMER_CC_TypeDef::CTRL

CC Channel Control Register

Definition at line 47 of file efm32wg_timer_cc.h .

Referenced by TIMER_InitCC() , and TIMER_Reset() .


The documentation for this struct was generated from the following file:
  • C:/repos/embsw_super_h1/platform/Device/SiliconLabs/EFM32WG/Include/ efm32wg_timer_cc.h