RTC_TypeDef Struct ReferenceDevices > EFM32WG_RTC
Definition at line 48
of file efm32wg_rtc.h
.
Data Fields | |
__IOM uint32_t | CNT |
__IOM uint32_t | COMP0 |
__IOM uint32_t | COMP1 |
__IOM uint32_t | CTRL |
__IOM uint32_t | FREEZE |
__IOM uint32_t | IEN |
__IM uint32_t | IF |
__IOM uint32_t | IFC |
__IOM uint32_t | IFS |
__IM uint32_t | SYNCBUSY |
Field Documentation
__IOM uint32_t RTC_TypeDef::CNT |
Counter Value Register
Definition at line 50
of file efm32wg_rtc.h
.
__IOM uint32_t RTC_TypeDef::COMP0 |
Compare Value Register 0
Definition at line 51
of file efm32wg_rtc.h
.
__IOM uint32_t RTC_TypeDef::COMP1 |
Compare Value Register 1
Definition at line 52
of file efm32wg_rtc.h
.
__IOM uint32_t RTC_TypeDef::CTRL |
Control Register
Definition at line 49
of file efm32wg_rtc.h
.
__IOM uint32_t RTC_TypeDef::FREEZE |
Freeze Register
Definition at line 58
of file efm32wg_rtc.h
.
__IOM uint32_t RTC_TypeDef::IEN |
Interrupt Enable Register
Definition at line 56
of file efm32wg_rtc.h
.
__IM uint32_t RTC_TypeDef::IF |
Interrupt Flag Register
Definition at line 53
of file efm32wg_rtc.h
.
__IOM uint32_t RTC_TypeDef::IFC |
Interrupt Flag Clear Register
Definition at line 55
of file efm32wg_rtc.h
.
__IOM uint32_t RTC_TypeDef::IFS |
Interrupt Flag Set Register
Definition at line 54
of file efm32wg_rtc.h
.
__IM uint32_t RTC_TypeDef::SYNCBUSY |
Synchronization Busy Register
Definition at line 59
of file efm32wg_rtc.h
.
The documentation for this struct was generated from the following file:
- C:/repos/embsw_super_h1/platform/Device/SiliconLabs/EFM32WG/Include/
efm32wg_rtc.h