ADC_TypeDef Struct ReferenceDevices > EFM32WG_ADC

Definition at line 48 of file efm32wg_adc.h .

Data Fields

__IOM uint32_t BIASPROG
__IOM uint32_t CAL
__IOM uint32_t CMD
__IOM uint32_t CTRL
__IOM uint32_t IEN
__IM uint32_t IF
__IOM uint32_t IFC
__IOM uint32_t IFS
uint32_t RESERVED0 [1]
__IOM uint32_t SCANCTRL
__IM uint32_t SCANDATA
__IM uint32_t SCANDATAP
__IOM uint32_t SINGLECTRL
__IM uint32_t SINGLEDATA
__IM uint32_t SINGLEDATAP
__IM uint32_t STATUS

Field Documentation

__IOM uint32_t ADC_TypeDef::BIASPROG

Bias Programming Register

Definition at line 65 of file efm32wg_adc.h .

Referenced by ADC_InitSingle() , and ADC_Reset() .

__IOM uint32_t ADC_TypeDef::CAL

Calibration Register

Definition at line 62 of file efm32wg_adc.h .

__IOM uint32_t ADC_TypeDef::CMD

Command Register

Definition at line 50 of file efm32wg_adc.h .

Referenced by ADC_Init() , ADC_InitScan() , ADC_InitSingle() , ADC_Reset() , and ADC_Start() .

__IOM uint32_t ADC_TypeDef::CTRL

Control Register

Definition at line 49 of file efm32wg_adc.h .

Referenced by ADC_Init() , ADC_InitScan() , ADC_InitSingle() , and ADC_Reset() .

__IOM uint32_t ADC_TypeDef::IEN

Interrupt Enable Register

Definition at line 54 of file efm32wg_adc.h .

Referenced by ADC_IntDisable() , ADC_IntEnable() , ADC_IntGetEnabled() , and ADC_Reset() .

__IM uint32_t ADC_TypeDef::IF

Interrupt Flag Register

Definition at line 55 of file efm32wg_adc.h .

Referenced by ADC_IntGet() , and ADC_IntGetEnabled() .

__IOM uint32_t ADC_TypeDef::IFC

Interrupt Flag Clear Register

Definition at line 57 of file efm32wg_adc.h .

Referenced by ADC_IntClear() , and ADC_Reset() .

__IOM uint32_t ADC_TypeDef::IFS

Interrupt Flag Set Register

Definition at line 56 of file efm32wg_adc.h .

Referenced by ADC_IntSet() .

uint32_t ADC_TypeDef::RESERVED0[1]

Reserved for future use

Definition at line 64 of file efm32wg_adc.h .

__IOM uint32_t ADC_TypeDef::SCANCTRL

Scan Control Register

Definition at line 53 of file efm32wg_adc.h .

Referenced by ADC_InitScan() , and ADC_Reset() .

__IM uint32_t ADC_TypeDef::SCANDATA

Scan Conversion Result Data

Definition at line 59 of file efm32wg_adc.h .

Referenced by ADC_DataScanGet() .

__IM uint32_t ADC_TypeDef::SCANDATAP

Scan Sequence Result Data Peek Register

Definition at line 61 of file efm32wg_adc.h .

Referenced by ADC_DataScanPeek() .

__IOM uint32_t ADC_TypeDef::SINGLECTRL

Single Sample Control Register

Definition at line 52 of file efm32wg_adc.h .

Referenced by ADC_InitSingle() , and ADC_Reset() .

__IM uint32_t ADC_TypeDef::SINGLEDATA

Single Conversion Result Data

Definition at line 58 of file efm32wg_adc.h .

Referenced by ADC_DataSingleGet() .

__IM uint32_t ADC_TypeDef::SINGLEDATAP

Single Conversion Result Data Peek Register

Definition at line 60 of file efm32wg_adc.h .

Referenced by ADC_DataSinglePeek() .

__IM uint32_t ADC_TypeDef::STATUS

Status Register

Definition at line 51 of file efm32wg_adc.h .

Referenced by ADC_InitScan() , and ADC_InitSingle() .


The documentation for this struct was generated from the following file:
  • C:/repos/embsw_super_h1/platform/Device/SiliconLabs/EFM32WG/Include/ efm32wg_adc.h