display.h File Reference
Display device interface.
- Version
 - 5.4.0
 
License
Copyright 2015 Silicon Labs, Inc. http://www.silabs.com
This file is licensed under the Silabs License Agreement. See the file "Silabs_License_Agreement.txt" for details. Before using this software for any purpose, you must agree to the terms of that agreement.
       Definition in file
       
        display.h
       
       .
      
       #include <stdbool.h>
      
      
       #include <stdint.h>
      
      
       #include "
       
        emstatus.h
       
       "
      
      
       #include "
       
        displayconfigall.h
       
       "
      
      
         Data Structures | 
       |
| struct | DISPLAY_Device_t | 
| struct | DISPLAY_Geometry_t | 
         Macros | 
       |
| #define | DISPLAY_EMSTATUS_INVALID_PARAMETER ( DISPLAY_EMSTATUS_BASE | 3) | 
| #define | DISPLAY_EMSTATUS_NOT_ENOUGH_MEMORY ( DISPLAY_EMSTATUS_BASE | 1) | 
| #define | DISPLAY_EMSTATUS_NOT_INITIALIZED ( DISPLAY_EMSTATUS_BASE | 5) | 
| #define | DISPLAY_EMSTATUS_NOT_SUPPORTED ( DISPLAY_EMSTATUS_BASE | 4) | 
| #define | DISPLAY_EMSTATUS_OK (0) | 
| #define | DISPLAY_EMSTATUS_OUT_OF_RANGE ( DISPLAY_EMSTATUS_BASE | 2) | 
         Typedefs | 
       |
| typedef enum DISPLAY_AddressMode_t | DISPLAY_AddressMode_t | 
| typedef enum DISPLAY_ColourMode_t | DISPLAY_ColourMode_t | 
| typedef struct DISPLAY_Device_t | DISPLAY_Device_t | 
| typedef struct DISPLAY_Geometry_t | DISPLAY_Geometry_t | 
| typedef void * | DISPLAY_PixelMatrix_t | 
| typedef EMSTATUS(* | pDisplayDeviceDriverInitFunction_t ) (void) | 
         Functions | 
       |
| EMSTATUS | DISPLAY_DeviceGet (int displayDeviceNo, DISPLAY_Device_t *device) | 
| 
         Get the display device data structure corresponding to the device number.
          | 
       |
| EMSTATUS | DISPLAY_DriverRefresh (void) | 
| 
         Refresh all DISPLAY devices.
          | 
       |
| EMSTATUS | DISPLAY_Init (void) | 
| 
         Initialize the DISPLAY module.
          | 
       |