RTC_TypeDef Struct ReferenceDevices > EZR32HG_RTC
       Definition at line
       
        48
       
       of file
       
        ezr32hg_rtc.h
       
       .
      
         Data Fields | 
       |
| __IOM uint32_t | CNT | 
| __IOM uint32_t | COMP0 | 
| __IOM uint32_t | COMP1 | 
| __IOM uint32_t | CTRL | 
| __IOM uint32_t | FREEZE | 
| __IOM uint32_t | IEN | 
| __IM uint32_t | IF | 
| __IOM uint32_t | IFC | 
| __IOM uint32_t | IFS | 
| __IM uint32_t | SYNCBUSY | 
Field Documentation
| __IOM uint32_t RTC_TypeDef::CNT | 
Counter Value Register
        Definition at line
        
         50
        
        of file
        
         ezr32hg_rtc.h
        
        .
       
| __IOM uint32_t RTC_TypeDef::COMP0 | 
Compare Value Register 0
        Definition at line
        
         51
        
        of file
        
         ezr32hg_rtc.h
        
        .
       
| __IOM uint32_t RTC_TypeDef::COMP1 | 
Compare Value Register 1
        Definition at line
        
         52
        
        of file
        
         ezr32hg_rtc.h
        
        .
       
| __IOM uint32_t RTC_TypeDef::CTRL | 
Control Register
        Definition at line
        
         49
        
        of file
        
         ezr32hg_rtc.h
        
        .
       
| __IOM uint32_t RTC_TypeDef::FREEZE | 
Freeze Register
        Definition at line
        
         58
        
        of file
        
         ezr32hg_rtc.h
        
        .
       
| __IOM uint32_t RTC_TypeDef::IEN | 
Interrupt Enable Register
        Definition at line
        
         56
        
        of file
        
         ezr32hg_rtc.h
        
        .
       
| __IM uint32_t RTC_TypeDef::IF | 
Interrupt Flag Register
        Definition at line
        
         53
        
        of file
        
         ezr32hg_rtc.h
        
        .
       
| __IOM uint32_t RTC_TypeDef::IFC | 
Interrupt Flag Clear Register
        Definition at line
        
         55
        
        of file
        
         ezr32hg_rtc.h
        
        .
       
| __IOM uint32_t RTC_TypeDef::IFS | 
Interrupt Flag Set Register
        Definition at line
        
         54
        
        of file
        
         ezr32hg_rtc.h
        
        .
       
| __IM uint32_t RTC_TypeDef::SYNCBUSY | 
Synchronization Busy Register
        Definition at line
        
         59
        
        of file
        
         ezr32hg_rtc.h
        
        .
       
The documentation for this struct was generated from the following file:
- 
       C:/repos/embsw_super_h1/platform/Device/SiliconLabs/EZR32HG/Include/
       
ezr32hg_rtc.h