LEUART_Init_TypeDef Struct ReferenceEMLIB > LEUART
Init structure.
       Definition at line
       
        99
       
       of file
       
        em_leuart.h
       
       .
      
      
       #include <
       
     
        em_leuart.h
       
       >
      
         Data Fields | 
       |
| uint32_t | baudrate | 
| LEUART_Databits_TypeDef | databits | 
| LEUART_Enable_TypeDef | enable | 
| LEUART_Parity_TypeDef | parity | 
| uint32_t | refFreq | 
| LEUART_Stopbits_TypeDef | stopbits | 
Field Documentation
| uint32_t LEUART_Init_TypeDef::baudrate | 
Desired baudrate.
        Definition at line
        
         110
        
        of file
        
         em_leuart.h
        
        .
       
Referenced by BSP_BccInit() , LEUART_Init() , RETARGET_SerialInit() , and UARTDRV_InitLeuart() .
| LEUART_Databits_TypeDef LEUART_Init_TypeDef::databits | 
Number of databits in frame.
        Definition at line
        
         113
        
        of file
        
         em_leuart.h
        
        .
       
Referenced by LEUART_Init() , and UARTDRV_InitLeuart() .
| LEUART_Enable_TypeDef LEUART_Init_TypeDef::enable | 
Specifies whether TX and/or RX shall be enabled when init completed.
        Definition at line
        
         101
        
        of file
        
         em_leuart.h
        
        .
       
Referenced by LEUART_Init() , RETARGET_SerialInit() , and UARTDRV_InitLeuart() .
| LEUART_Parity_TypeDef LEUART_Init_TypeDef::parity | 
Parity mode to use.
        Definition at line
        
         116
        
        of file
        
         em_leuart.h
        
        .
       
Referenced by LEUART_Init() , and UARTDRV_InitLeuart() .
| uint32_t LEUART_Init_TypeDef::refFreq | 
LEUART reference clock assumed when configuring baudrate setup. Set it to 0 if currently configurated reference clock shall be used.
        Definition at line
        
         107
        
        of file
        
         em_leuart.h
        
        .
       
Referenced by LEUART_Init() .
| LEUART_Stopbits_TypeDef LEUART_Init_TypeDef::stopbits | 
Number of stopbits to use.
        Definition at line
        
         119
        
        of file
        
         em_leuart.h
        
        .
       
Referenced by LEUART_Init() , and UARTDRV_InitLeuart() .
The documentation for this struct was generated from the following file:
- 
       C:/repos/embsw_super_h1/platform/emlib/inc/
       
em_leuart.h