RMU_TypeDef Struct ReferenceDevices > EZR32HG_RMU
       Definition at line
       
        48
       
       of file
       
        ezr32hg_rmu.h
       
       .
      
         Data Fields | 
       |
| __OM uint32_t | CMD | 
| __IOM uint32_t | CTRL | 
| __IM uint32_t | RSTCAUSE | 
Field Documentation
| __OM uint32_t RMU_TypeDef::CMD | 
Command Register
        Definition at line
        
         51
        
        of file
        
         ezr32hg_rmu.h
        
        .
       
| __IOM uint32_t RMU_TypeDef::CTRL | 
Control Register
        Definition at line
        
         49
        
        of file
        
         ezr32hg_rmu.h
        
        .
       
| __IM uint32_t RMU_TypeDef::RSTCAUSE | 
Reset Cause Register
        Definition at line
        
         50
        
        of file
        
         ezr32hg_rmu.h
        
        .
       
The documentation for this struct was generated from the following file:
- 
       C:/repos/embsw_super_h1/platform/Device/SiliconLabs/EZR32HG/Include/
       
ezr32hg_rmu.h