DMA_TypeDef Struct ReferenceDevices > EZR32HG_DMA
       Definition at line
       
        48
       
       of file
       
        ezr32hg_dma.h
       
       .
      
         Data Fields | 
       |
| __IM uint32_t | ALTCTRLBASE | 
| DMA_CH_TypeDef | CH [6] | 
| __OM uint32_t | CHALTC | 
| __IOM uint32_t | CHALTS | 
| __OM uint32_t | CHENC | 
| __IOM uint32_t | CHENS | 
| __OM uint32_t | CHPRIC | 
| __IOM uint32_t | CHPRIS | 
| __OM uint32_t | CHREQMASKC | 
| __IOM uint32_t | CHREQMASKS | 
| __IM uint32_t | CHREQSTATUS | 
| __IM uint32_t | CHSREQSTATUS | 
| __OM uint32_t | CHSWREQ | 
| __OM uint32_t | CHUSEBURSTC | 
| __IOM uint32_t | CHUSEBURSTS | 
| __IM uint32_t | CHWAITSTATUS | 
| __OM uint32_t | CONFIG | 
| __IOM uint32_t | CTRLBASE | 
| __IOM uint32_t | ERRORC | 
| __IOM uint32_t | IEN | 
| __IM uint32_t | IF | 
| __IOM uint32_t | IFC | 
| __IOM uint32_t | IFS | 
| uint32_t | RESERVED0 [3] | 
| uint32_t | RESERVED1 [880] | 
| uint32_t | RESERVED2 [1] | 
| uint32_t | RESERVED3 [121] | 
| uint32_t | RESERVED4 [60] | 
| __IM uint32_t | STATUS | 
Field Documentation
| __IM uint32_t DMA_TypeDef::ALTCTRLBASE | 
Channel Alternate Control Data Base Pointer Register
        Definition at line
        
         52
        
        of file
        
         ezr32hg_dma.h
        
        .
       
| DMA_CH_TypeDef DMA_TypeDef::CH[6] | 
Channel registers
        Definition at line
        
         80
        
        of file
        
         ezr32hg_dma.h
        
        .
       
| __OM uint32_t DMA_TypeDef::CHALTC | 
Channel Alternate Clear Register
        Definition at line
        
         62
        
        of file
        
         ezr32hg_dma.h
        
        .
       
| __IOM uint32_t DMA_TypeDef::CHALTS | 
Channel Alternate Set Register
        Definition at line
        
         61
        
        of file
        
         ezr32hg_dma.h
        
        .
       
| __OM uint32_t DMA_TypeDef::CHENC | 
Channel Enable Clear Register
        Definition at line
        
         60
        
        of file
        
         ezr32hg_dma.h
        
        .
       
| __IOM uint32_t DMA_TypeDef::CHENS | 
Channel Enable Set Register
        Definition at line
        
         59
        
        of file
        
         ezr32hg_dma.h
        
        .
       
| __OM uint32_t DMA_TypeDef::CHPRIC | 
Channel Priority Clear Register
        Definition at line
        
         64
        
        of file
        
         ezr32hg_dma.h
        
        .
       
| __IOM uint32_t DMA_TypeDef::CHPRIS | 
Channel Priority Set Register
        Definition at line
        
         63
        
        of file
        
         ezr32hg_dma.h
        
        .
       
| __OM uint32_t DMA_TypeDef::CHREQMASKC | 
Channel Request Mask Clear Register
        Definition at line
        
         58
        
        of file
        
         ezr32hg_dma.h
        
        .
       
| __IOM uint32_t DMA_TypeDef::CHREQMASKS | 
Channel Request Mask Set Register
        Definition at line
        
         57
        
        of file
        
         ezr32hg_dma.h
        
        .
       
| __IM uint32_t DMA_TypeDef::CHREQSTATUS | 
Channel Request Status
        Definition at line
        
         69
        
        of file
        
         ezr32hg_dma.h
        
        .
       
| __IM uint32_t DMA_TypeDef::CHSREQSTATUS | 
Channel Single Request Status
        Definition at line
        
         71
        
        of file
        
         ezr32hg_dma.h
        
        .
       
| __OM uint32_t DMA_TypeDef::CHSWREQ | 
Channel Software Request Register
        Definition at line
        
         54
        
        of file
        
         ezr32hg_dma.h
        
        .
       
| __OM uint32_t DMA_TypeDef::CHUSEBURSTC | 
Channel Useburst Clear Register
        Definition at line
        
         56
        
        of file
        
         ezr32hg_dma.h
        
        .
       
| __IOM uint32_t DMA_TypeDef::CHUSEBURSTS | 
Channel Useburst Set Register
        Definition at line
        
         55
        
        of file
        
         ezr32hg_dma.h
        
        .
       
| __IM uint32_t DMA_TypeDef::CHWAITSTATUS | 
Channel Wait on Request Status Register
        Definition at line
        
         53
        
        of file
        
         ezr32hg_dma.h
        
        .
       
| __OM uint32_t DMA_TypeDef::CONFIG | 
DMA Configuration Register
        Definition at line
        
         50
        
        of file
        
         ezr32hg_dma.h
        
        .
       
| __IOM uint32_t DMA_TypeDef::CTRLBASE | 
Channel Control Data Base Pointer Register
        Definition at line
        
         51
        
        of file
        
         ezr32hg_dma.h
        
        .
       
| __IOM uint32_t DMA_TypeDef::ERRORC | 
Bus Error Clear Register
        Definition at line
        
         66
        
        of file
        
         ezr32hg_dma.h
        
        .
       
| __IOM uint32_t DMA_TypeDef::IEN | 
Interrupt Enable register
        Definition at line
        
         77
        
        of file
        
         ezr32hg_dma.h
        
        .
       
| __IM uint32_t DMA_TypeDef::IF | 
Interrupt Flag Register
        Definition at line
        
         74
        
        of file
        
         ezr32hg_dma.h
        
        .
       
| __IOM uint32_t DMA_TypeDef::IFC | 
Interrupt Flag Clear Register
        Definition at line
        
         76
        
        of file
        
         ezr32hg_dma.h
        
        .
       
| __IOM uint32_t DMA_TypeDef::IFS | 
Interrupt Flag Set Register
        Definition at line
        
         75
        
        of file
        
         ezr32hg_dma.h
        
        .
       
| uint32_t DMA_TypeDef::RESERVED0[3] | 
Reserved for future use
        Definition at line
        
         65
        
        of file
        
         ezr32hg_dma.h
        
        .
       
| uint32_t DMA_TypeDef::RESERVED1[880] | 
Reserved for future use
        Definition at line
        
         68
        
        of file
        
         ezr32hg_dma.h
        
        .
       
| uint32_t DMA_TypeDef::RESERVED2[1] | 
Reserved for future use
        Definition at line
        
         70
        
        of file
        
         ezr32hg_dma.h
        
        .
       
| uint32_t DMA_TypeDef::RESERVED3[121] | 
Reserved for future use
        Definition at line
        
         73
        
        of file
        
         ezr32hg_dma.h
        
        .
       
| uint32_t DMA_TypeDef::RESERVED4[60] | 
Reserved registers
        Definition at line
        
         79
        
        of file
        
         ezr32hg_dma.h
        
        .
       
| __IM uint32_t DMA_TypeDef::STATUS | 
DMA Status Registers
        Definition at line
        
         49
        
        of file
        
         ezr32hg_dma.h
        
        .
       
The documentation for this struct was generated from the following file:
- 
       C:/repos/embsw_super_h1/platform/Device/SiliconLabs/EZR32HG/Include/
       
ezr32hg_dma.h