EMU_TypeDef Struct ReferenceDevices > EZR32HG_EMU
       Definition at line
       
        48
       
       of file
       
        ezr32hg_emu.h
       
       .
      
         Data Fields | 
       |
| __IOM uint32_t | AUXCTRL | 
| __IOM uint32_t | CTRL | 
| __IOM uint32_t | LOCK | 
| uint32_t | RESERVED0 [1] | 
| uint32_t | RESERVED1 [6] | 
Field Documentation
| __IOM uint32_t EMU_TypeDef::AUXCTRL | 
Auxiliary Control Register
        Definition at line
        
         55
        
        of file
        
         ezr32hg_emu.h
        
        .
       
| __IOM uint32_t EMU_TypeDef::CTRL | 
Control Register
        Definition at line
        
         49
        
        of file
        
         ezr32hg_emu.h
        
        .
       
| __IOM uint32_t EMU_TypeDef::LOCK | 
Configuration Lock Register
        Definition at line
        
         52
        
        of file
        
         ezr32hg_emu.h
        
        .
       
| uint32_t EMU_TypeDef::RESERVED0[1] | 
Reserved for future use
        Definition at line
        
         51
        
        of file
        
         ezr32hg_emu.h
        
        .
       
| uint32_t EMU_TypeDef::RESERVED1[6] | 
Reserved for future use
        Definition at line
        
         54
        
        of file
        
         ezr32hg_emu.h
        
        .
       
The documentation for this struct was generated from the following file:
- 
       C:/repos/embsw_super_h1/platform/Device/SiliconLabs/EZR32HG/Include/
       
ezr32hg_emu.h