SegmentLcdKit Drivers
         Enumerations | 
       |
| enum | 
         
          SegmentLCD_BlockMode_TypeDef
         
         {
          segmentLCDBlockModeBlank = SEGMENT_LCD_BLOCK_MODE_BLANK, segmentLCDBlockModeFill = SEGMENT_LCD_BLOCK_MODE_FILL, segmentLCDBlockModeOutline = SEGMENT_LCD_BLOCK_MODE_OUTLINE, segmentLCDBlockModeOutlineFill = SEGMENT_LCD_BLOCK_MODE_OUTLINE_FILL }  | 
       
         Functions | 
       |
| void | SegmentLCD_AllOff (void) | 
| 
         Disable all segments.
          | 
       |
| void | SegmentLCD_AllOn (void) | 
| 
         Enable all segments.
          | 
       |
| void | SegmentLCD_AlphaNumberOff (void) | 
| 
         Turn all segments on alpha characters in display off.
          | 
       |
| void | SegmentLCD_ARing (int anum, int on) | 
| 
         Light up or shut off Ring of Indicators.
          | 
       |
| void | SegmentLCD_Battery (int batteryLevel) | 
| 
         Light up or shut off Battery Indicator.
          | 
       |
| void | SegmentLCD_Block ( SegmentLCD_BlockMode_TypeDef topMode[SEGMENT_LCD_NUM_BLOCK_COLUMNS], SegmentLCD_BlockMode_TypeDef botMode[SEGMENT_LCD_NUM_BLOCK_COLUMNS]) | 
| void | SegmentLCD_Disable (void) | 
| 
         Disables LCD controller.
          | 
       |
| void | SegmentLCD_EnergyMode (int em, int on) | 
| 
         Light up or shut off Energy Mode indicator.
          | 
       |
| void | SegmentLCD_Init (bool useBoost) | 
| 
         Segment LCD Initialization routine for EFM32 STK display.
          | 
       |
| void | SegmentLCD_LowerHex (uint32_t num) | 
| 
         Write a hexadecimal number on lower alphanumeric part of Segment LCD display.
          | 
       |
| void | SegmentLCD_LowerNumber (int num) | 
| 
         Write number on lower alphanumeric part of Segment LCD display.
          | 
       |
| void | SegmentLCD_Number (int value) | 
| 
         Write number on numeric part on Segment LCD display.
          | 
       |
| void | SegmentLCD_NumberOff (void) | 
| 
         Turn all segments on numeric digits in display off.
          | 
       |
| void | SegmentLCD_Symbol (lcdSymbol s, int on) | 
| 
         Light up or shut off various symbols on Segment LCD.
          | 
       |
| void | SegmentLCD_UnsignedHex (uint32_t value) | 
| 
         Write hexadecimal number on numeric part on Segment LCD display.
          | 
       |
| void | SegmentLCD_Write (const char *string) | 
| 
         Write text on LCD display.
          | 
       |
Enumeration Type Documentation
Function Documentation
| void SegmentLCD_ARing | ( | int | 
           
            anum,
           
           | 
         
| int | 
           
            on
           
           | 
         ||
| ) | 
Light up or shut off Ring of Indicators.
- Parameters
 - 
         
anum"Segment number" on "Ring", range 0 - 7 onZero is off, non-zero is on  
        Definition at line
        
         1361
        
        of file
        
         segmentlcd.c
        
        .
       
References MCU_DISPLAY::ARing , ARING_TypeDef::bit , and ARING_TypeDef::com .
| void SegmentLCD_Battery | ( | int | 
           
            batteryLevel
           
           | 
          ) | 
Light up or shut off Battery Indicator.
- Parameters
 - 
         
batteryLevelBattery Level, 0 to 4 (0 turns all off)  
        Definition at line
        
         1379
        
        of file
        
         segmentlcd.c
        
        .
       
References MCU_DISPLAY::Battery , BATTERY_TypeDef::bit , and BATTERY_TypeDef::com .
| void SegmentLCD_EnergyMode | ( | int | 
           
            em,
           
           | 
         
| int | 
           
            on
           
           | 
         ||
| ) | 
Light up or shut off Energy Mode indicator.
- Parameters
 - 
         
emEnergy Mode numer 0 to 4 onZero is off, non-zero is on  
        Definition at line
        
         1406
        
        of file
        
         segmentlcd.c
        
        .
       
References EM_TypeDef::bit , EM_TypeDef::com , and MCU_DISPLAY::EMode .
| void SegmentLCD_Init | ( | bool | 
           
            useBoost
           
           | 
          ) | 
Segment LCD Initialization routine for EFM32 STK display.
- Parameters
 - 
         
useBoostSet to use voltage boost  
        Definition at line
        
         448
        
        of file
        
         segmentlcd.c
        
        .
       
References CMU , CMU_ClockDivSet() , CMU_ClockEnable() , CMU_ClockSelectSet() , CMU_LCDClkFDIVSet() , cmuClock_LFA , cmuSelect_LFRCO , and SegmentLCD_AllOff() .
| void SegmentLCD_LowerHex | ( | uint32_t | 
           
            num
           
           | 
          ) | 
Write a hexadecimal number on lower alphanumeric part of Segment LCD display.
- Parameters
 - 
         
numHexadecimal number value to put on display, in range 0 to 0x0FFFFFFF  
        Definition at line
        
         502
        
        of file
        
         segmentlcd.c
        
        .
       
References SegmentLCD_Symbol() , and SegmentLCD_Write() .
| void SegmentLCD_LowerNumber | ( | int | 
           
            num
           
           | 
          ) | 
Write number on lower alphanumeric part of Segment LCD display.
- Parameters
 - 
         
numNumeric value to put on display, in range -9999999 to +9999999  
        Definition at line
        
         535
        
        of file
        
         segmentlcd.c
        
        .
       
References SegmentLCD_Symbol() , and SegmentLCD_Write() .
| void SegmentLCD_Number | ( | int | 
           
            value
           
           | 
          ) | 
Write number on numeric part on Segment LCD display.
- Parameters
 - 
         
valueNumeric value to put on display, in range -999 to +9999  
        Definition at line
        
         580
        
        of file
        
         segmentlcd.c
        
        .
       
References NUMBER_TypeDef::bit , NUMBER_TypeDef::com , MCU_DISPLAY::Number , Segment_Numbers , and SegmentLCD_NumberOff() .
| void SegmentLCD_Symbol | ( | lcdSymbol | 
           
            s,
           
           | 
         
| int | 
           
            on
           
           | 
         ||
| ) | 
Light up or shut off various symbols on Segment LCD.
- Parameters
 - 
         
sWhich symbol to turn on or off onZero is off, non-zero is on  
        Definition at line
        
         661
        
        of file
        
         segmentlcd.c
        
        .
       
Referenced by SegmentLCD_LowerHex() , and SegmentLCD_LowerNumber() .
| void SegmentLCD_UnsignedHex | ( | uint32_t | 
           
            value
           
           | 
          ) | 
Write hexadecimal number on numeric part on Segment LCD display.
- Parameters
 - 
         
valueNumeric value to put on display  
        Definition at line
        
         1015
        
        of file
        
         segmentlcd.c
        
        .
       
References NUMBER_TypeDef::bit , NUMBER_TypeDef::com , MCU_DISPLAY::Number , Segment_Numbers , and SegmentLCD_NumberOff() .
| void SegmentLCD_Write | ( | const char * | 
           
            string
           
           | 
          ) | 
Write text on LCD display.
- Parameters
 - 
         
stringText string to show on display  
        Definition at line
        
         1062
        
        of file
        
         segmentlcd.c
        
        .
       
References CHAR_TypeDef::bit , CHAR_TypeDef::com , Segment_Alphabet , SegmentLCD_AlphaNumberOff() , and MCU_DISPLAY::Text .
Referenced by SegmentLCD_LowerHex() , and SegmentLCD_LowerNumber() .