ARING_TypeDef Struct Reference

Defines segment COM and BIT fields for A-wheel (suited for Anim)

Definition at line 90 of file segmentlcd.c.

Data Fields

uint8_t bit [8]
 
uint8_t com [8]
 

Field Documentation

uint8_t ARING_TypeDef::bit[8]

LCD bit number

Definition at line 92 of file segmentlcd.c.

Referenced by SegmentLCD_ARing().

uint8_t ARING_TypeDef::com[8]

LCD COM line (for multiplexing)

Definition at line 91 of file segmentlcd.c.

Referenced by SegmentLCD_ARing().


The documentation for this struct was generated from the following file:
  • C:/repos/embsw_super_h1/hardware/kit/common/drivers/segmentlcd.c