PRS_TypeDef Struct ReferenceDevices > EZR32HG_PRS
       Definition at line
       
        48
       
       of file
       
        ezr32hg_prs.h
       
       .
      
         Data Fields | 
       |
| PRS_CH_TypeDef | CH [6] | 
| uint32_t | RESERVED0 [1] | 
| uint32_t | RESERVED1 [6] | 
| __IOM uint32_t | ROUTE | 
| __IOM uint32_t | SWLEVEL | 
| __IOM uint32_t | SWPULSE | 
| __IOM uint32_t | TRACECTRL | 
Field Documentation
| PRS_CH_TypeDef PRS_TypeDef::CH[6] | 
Channel registers
        Definition at line
        
         54
        
        of file
        
         ezr32hg_prs.h
        
        .
       
| uint32_t PRS_TypeDef::RESERVED0[1] | 
Reserved registers
        Definition at line
        
         53
        
        of file
        
         ezr32hg_prs.h
        
        .
       
| uint32_t PRS_TypeDef::RESERVED1[6] | 
Reserved for future use
        Definition at line
        
         56
        
        of file
        
         ezr32hg_prs.h
        
        .
       
| __IOM uint32_t PRS_TypeDef::ROUTE | 
I/O Routing Register
        Definition at line
        
         51
        
        of file
        
         ezr32hg_prs.h
        
        .
       
| __IOM uint32_t PRS_TypeDef::SWLEVEL | 
Software Level Register
        Definition at line
        
         50
        
        of file
        
         ezr32hg_prs.h
        
        .
       
| __IOM uint32_t PRS_TypeDef::SWPULSE | 
Software Pulse Register
        Definition at line
        
         49
        
        of file
        
         ezr32hg_prs.h
        
        .
       
| __IOM uint32_t PRS_TypeDef::TRACECTRL | 
MTB Trace Control Register
        Definition at line
        
         57
        
        of file
        
         ezr32hg_prs.h
        
        .
       
The documentation for this struct was generated from the following file:
- 
       C:/repos/embsw_super_h1/platform/Device/SiliconLabs/EZR32HG/Include/
       
ezr32hg_prs.h