ADC_Init_TypeDef Struct ReferenceEMLIB > ADC
ADC init structure, common for single conversion and scan sequence.
       Definition at line
       
        781
       
       of file
       
        em_adc.h
       
       .
      
      
       #include <
       
     
        em_adc.h
       
       >
      
         Data Fields | 
       |
| ADC_LPFilter_TypeDef | lpfMode | 
| ADC_OvsRateSel_TypeDef | ovsRateSel | 
| uint8_t | prescale | 
| bool | tailgate | 
| uint8_t | timebase | 
| ADC_Warmup_TypeDef | warmUpMode | 
Field Documentation
| ADC_LPFilter_TypeDef ADC_Init_TypeDef::lpfMode | 
Lowpass or decoupling capacitor filter to use.
        Definition at line
        
         790
        
        of file
        
         em_adc.h
        
        .
       
Referenced by ADC_Init() .
| ADC_OvsRateSel_TypeDef ADC_Init_TypeDef::ovsRateSel | 
Oversampling rate select. In order to have any effect, oversampling must be enabled for single/scan mode.
        Definition at line
        
         786
        
        of file
        
         em_adc.h
        
        .
       
Referenced by ADC_Init() , and TOUCH_Init() .
| uint8_t ADC_Init_TypeDef::prescale | 
Clock division factor N, ADC clock = HFPERCLK / (N + 1).
        Definition at line
        
         806
        
        of file
        
         em_adc.h
        
        .
       
Referenced by ADC_Init() , adcInit() , MIC_init() , and TOUCH_Init() .
| bool ADC_Init_TypeDef::tailgate | 
Enable/disable conversion tailgating.
        Definition at line
        
         809
        
        of file
        
         em_adc.h
        
        .
       
Referenced by ADC_Init() .
| uint8_t ADC_Init_TypeDef::timebase | 
Timebase used for ADC warm up. Select N to give (N+1)HFPERCLK cycles. (Additional delay is added for bandgap references, please refer to the reference manual.) Normally, N should be selected so that the timebase is at least 1 us. See ADC_TimebaseCalc() for a way to obtain a suggested timebase of at least 1 us.
        Definition at line
        
         803
        
        of file
        
         em_adc.h
        
        .
       
Referenced by ADC_Init() , adcInit() , and MIC_init() .
| ADC_Warmup_TypeDef ADC_Init_TypeDef::warmUpMode | 
The documentation for this struct was generated from the following file:
- 
       C:/repos/embsw_super_h1/platform/emlib/inc/
       
em_adc.h