USARTEMLIB
Detailed Description
Universal Synchronous/Asynchronous Receiver/Transmitter Peripheral API.
The Universal Synchronous/Asynchronous Receiver/Transmitter (USART) is a very flexible serial I/O module. It supports full duplex asynchronous UART communication as well as RS-485, SPI, MicroWire and 3-wire. It can also interface with ISO7816 Smart-Cards, and IrDA devices.
The USART has a wide selection of operating modes, frame formats and baud rates. All features are supported through the API of this module.
Triple buffering and DMA support makes high data-rates possible with minimal CPU intervention and it is possible to transmit and receive large frames while the MCU remains in EM1 Sleep.
This module does not support DMA configuration. The UARTDRV and SPIDRV drivers provide full support for DMA and more.
The following steps are necessary for basic operation:
Clock enable:
To initialize the USART for asynchronous operation (eg. UART):
To initialize the USART for synchronous operation (eg. SPI):
After pins are assigned for the application/board, enable pins at the desired location. Available locations can be obtained from the Pin Definitions section in the datasheet.
- Note
- UART hardware flow control is not directly supported in hardware on _SILICON_LABS_32B_SERIES_0 parts.
- UARTDRV supports all types of UART flow control. Software assisted hardware flow control is available for parts without true UART hardware flow control.
Data Structures |
|
| struct | USART_InitAsync_TypeDef |
| struct | USART_InitI2s_TypeDef |
| struct | USART_InitIrDA_TypeDef |
| struct | USART_InitSync_TypeDef |
| struct | USART_PrsTriggerInit_TypeDef |
Macros |
|
| #define | USART_INITASYNC_DEFAULT |
| #define | USART_INITI2S_DEFAULT |
| #define | USART_INITIRDA_DEFAULT |
| #define | USART_INITPRSTRIGGER_DEFAULT |
| #define | USART_INITSYNC_DEFAULT |
Enumerations |
|
| enum |
USART_ClockMode_TypeDef
{
usartClockMode0 = USART_CTRL_CLKPOL_IDLELOW | USART_CTRL_CLKPHA_SAMPLELEADING, usartClockMode1 = USART_CTRL_CLKPOL_IDLELOW | USART_CTRL_CLKPHA_SAMPLETRAILING, usartClockMode2 = USART_CTRL_CLKPOL_IDLEHIGH | USART_CTRL_CLKPHA_SAMPLELEADING, usartClockMode3 = USART_CTRL_CLKPOL_IDLEHIGH | USART_CTRL_CLKPHA_SAMPLETRAILING } |
| enum |
USART_Databits_TypeDef
{
usartDatabits4 = USART_FRAME_DATABITS_FOUR, usartDatabits5 = USART_FRAME_DATABITS_FIVE, usartDatabits6 = USART_FRAME_DATABITS_SIX, usartDatabits7 = USART_FRAME_DATABITS_SEVEN, usartDatabits8 = USART_FRAME_DATABITS_EIGHT, usartDatabits9 = USART_FRAME_DATABITS_NINE, usartDatabits10 = USART_FRAME_DATABITS_TEN, usartDatabits11 = USART_FRAME_DATABITS_ELEVEN, usartDatabits12 = USART_FRAME_DATABITS_TWELVE, usartDatabits13 = USART_FRAME_DATABITS_THIRTEEN, usartDatabits14 = USART_FRAME_DATABITS_FOURTEEN, usartDatabits15 = USART_FRAME_DATABITS_FIFTEEN, usartDatabits16 = USART_FRAME_DATABITS_SIXTEEN } |
| enum |
USART_Enable_TypeDef
{
usartDisable = 0x0, usartEnableRx = USART_CMD_RXEN, usartEnableTx = USART_CMD_TXEN, usartEnable = (USART_CMD_RXEN | USART_CMD_TXEN) } |
| enum |
USART_I2sFormat_TypeDef
{
usartI2sFormatW32D32 = USART_I2SCTRL_FORMAT_W32D32, usartI2sFormatW32D24M = USART_I2SCTRL_FORMAT_W32D24M, usartI2sFormatW32D24 = USART_I2SCTRL_FORMAT_W32D24, usartI2sFormatW32D16 = USART_I2SCTRL_FORMAT_W32D16, usartI2sFormatW32D8 = USART_I2SCTRL_FORMAT_W32D8, usartI2sFormatW16D16 = USART_I2SCTRL_FORMAT_W16D16, usartI2sFormatW16D8 = USART_I2SCTRL_FORMAT_W16D8, usartI2sFormatW8D8 = USART_I2SCTRL_FORMAT_W8D8 } |
| enum |
USART_I2sJustify_TypeDef
{
usartI2sJustifyLeft = USART_I2SCTRL_JUSTIFY_LEFT, usartI2sJustifyRight = USART_I2SCTRL_JUSTIFY_RIGHT } |
| enum |
USART_IrDAPrsSel_Typedef
{
usartIrDAPrsCh0 = USART_IRCTRL_IRPRSSEL_PRSCH0, usartIrDAPrsCh1 = USART_IRCTRL_IRPRSSEL_PRSCH1, usartIrDAPrsCh2 = USART_IRCTRL_IRPRSSEL_PRSCH2, usartIrDAPrsCh3 = USART_IRCTRL_IRPRSSEL_PRSCH3, usartIrDAPrsCh4 = USART_IRCTRL_IRPRSSEL_PRSCH4, usartIrDAPrsCh5 = USART_IRCTRL_IRPRSSEL_PRSCH5 } |
| enum |
USART_IrDAPw_Typedef
{
usartIrDAPwONE = USART_IRCTRL_IRPW_ONE, usartIrDAPwTWO = USART_IRCTRL_IRPW_TWO, usartIrDAPwTHREE = USART_IRCTRL_IRPW_THREE, usartIrDAPwFOUR = USART_IRCTRL_IRPW_FOUR } |
| enum |
USART_OVS_TypeDef
{
usartOVS16 = USART_CTRL_OVS_X16, usartOVS8 = USART_CTRL_OVS_X8, usartOVS6 = USART_CTRL_OVS_X6, usartOVS4 = USART_CTRL_OVS_X4 } |
| enum |
USART_Parity_TypeDef
{
usartNoParity = USART_FRAME_PARITY_NONE, usartEvenParity = USART_FRAME_PARITY_EVEN, usartOddParity = USART_FRAME_PARITY_ODD } |
| enum |
USART_PrsRxCh_TypeDef
{
usartPrsRxCh0 = USART_INPUT_RXPRSSEL_PRSCH0, usartPrsRxCh1 = USART_INPUT_RXPRSSEL_PRSCH1, usartPrsRxCh2 = USART_INPUT_RXPRSSEL_PRSCH2, usartPrsRxCh3 = USART_INPUT_RXPRSSEL_PRSCH3 } |
| enum |
USART_PrsTriggerCh_TypeDef
{
usartPrsTriggerCh0 = USART_TRIGCTRL_TSEL_PRSCH0, usartPrsTriggerCh1 = USART_TRIGCTRL_TSEL_PRSCH1, usartPrsTriggerCh2 = USART_TRIGCTRL_TSEL_PRSCH2, usartPrsTriggerCh3 = USART_TRIGCTRL_TSEL_PRSCH3 } |
| enum |
USART_Stopbits_TypeDef
{
usartStopbits0p5 = USART_FRAME_STOPBITS_HALF, usartStopbits1 = USART_FRAME_STOPBITS_ONE, usartStopbits1p5 = USART_FRAME_STOPBITS_ONEANDAHALF, usartStopbits2 = USART_FRAME_STOPBITS_TWO } |
Functions |
|
| void | USART_BaudrateAsyncSet ( USART_TypeDef *usart, uint32_t refFreq, uint32_t baudrate, USART_OVS_TypeDef ovs) |
|
Configure USART/UART operating in asynchronous mode to use a given baudrate (or as close as possible to specified baudrate).
|
|
| uint32_t | USART_BaudrateCalc (uint32_t refFreq, uint32_t clkdiv, bool syncmode, USART_OVS_TypeDef ovs) |
|
Calculate baudrate for USART/UART given reference frequency, clock division and oversampling rate (if async mode).
|
|
| uint32_t | USART_BaudrateGet ( USART_TypeDef *usart) |
|
Get current baudrate for USART/UART.
|
|
| void | USART_BaudrateSyncSet ( USART_TypeDef *usart, uint32_t refFreq, uint32_t baudrate) |
|
Configure USART operating in synchronous mode to use a given baudrate (or as close as possible to specified baudrate).
|
|
| void | USART_Enable ( USART_TypeDef *usart, USART_Enable_TypeDef enable) |
|
Enable/disable USART/UART receiver and/or transmitter.
|
|
| void | USART_InitAsync ( USART_TypeDef *usart, const USART_InitAsync_TypeDef *init) |
|
Init USART/UART for normal asynchronous mode.
|
|
| void | USART_InitI2s ( USART_TypeDef *usart, USART_InitI2s_TypeDef *init) |
|
Init USART for I2S mode.
|
|
| __STATIC_INLINE void | USART_InitIrDA (const USART_InitIrDA_TypeDef *init) |
|
Init DEFAULT_IRDA_USART for asynchronous IrDA mode.
|
|
| void | USART_InitPrsTrigger ( USART_TypeDef *usart, const USART_PrsTriggerInit_TypeDef *init) |
|
Initialize automatic transmissions using PRS channel as trigger.
|
|
| void | USART_InitSync ( USART_TypeDef *usart, const USART_InitSync_TypeDef *init) |
|
Init USART for synchronous mode.
|
|
| __STATIC_INLINE void | USART_IntClear ( USART_TypeDef *usart, uint32_t flags) |
|
Clear one or more pending USART interrupts.
|
|
| __STATIC_INLINE void | USART_IntDisable ( USART_TypeDef *usart, uint32_t flags) |
|
Disable one or more USART interrupts.
|
|
| __STATIC_INLINE void | USART_IntEnable ( USART_TypeDef *usart, uint32_t flags) |
|
Enable one or more USART interrupts.
|
|
| __STATIC_INLINE uint32_t | USART_IntGet ( USART_TypeDef *usart) |
|
Get pending USART interrupt flags.
|
|
| __STATIC_INLINE uint32_t | USART_IntGetEnabled ( USART_TypeDef *usart) |
|
Get enabled and pending USART interrupt flags. Useful for handling more interrupt sources in the same interrupt handler.
|
|
| __STATIC_INLINE void | USART_IntSet ( USART_TypeDef *usart, uint32_t flags) |
|
Set one or more pending USART interrupts from SW.
|
|
| void | USART_Reset ( USART_TypeDef *usart) |
|
Reset USART/UART to same state as after a HW reset.
|
|
| uint8_t | USART_Rx ( USART_TypeDef *usart) |
|
Receive one 4-8 bit frame, (or part of 10-16 bit frame).
|
|
| __STATIC_INLINE uint8_t | USART_RxDataGet ( USART_TypeDef *usart) |
|
Receive one 4-8 bit frame, (or part of 10-16 bit frame).
|
|
| __STATIC_INLINE uint16_t | USART_RxDataXGet ( USART_TypeDef *usart) |
|
Receive one 4-9 bit frame, (or part of 10-16 bit frame) with extended information.
|
|
| uint16_t | USART_RxDouble ( USART_TypeDef *usart) |
|
Receive two 4-8 bit frames, or one 10-16 bit frame.
|
|
| uint32_t | USART_RxDoubleExt ( USART_TypeDef *usart) |
|
Receive two 4-9 bit frames, or one 10-16 bit frame with extended information.
|
|
| __STATIC_INLINE uint16_t | USART_RxDoubleGet ( USART_TypeDef *usart) |
|
Receive two 4-8 bit frames, or one 10-16 bit frame.
|
|
| __STATIC_INLINE uint32_t | USART_RxDoubleXGet ( USART_TypeDef *usart) |
|
Receive two 4-9 bit frames, or one 10-16 bit frame with extended information.
|
|
| uint16_t | USART_RxExt ( USART_TypeDef *usart) |
|
Receive one 4-9 bit frame, (or part of 10-16 bit frame) with extended information.
|
|
| uint8_t | USART_SpiTransfer ( USART_TypeDef *usart, uint8_t data) |
|
Perform one 8 bit frame SPI transfer.
|
|
| __STATIC_INLINE uint32_t | USART_StatusGet ( USART_TypeDef *usart) |
|
Get USART STATUS register.
|
|
| void | USART_Tx ( USART_TypeDef *usart, uint8_t data) |
|
Transmit one 4-9 bit frame.
|
|
| void | USART_TxDouble ( USART_TypeDef *usart, uint16_t data) |
|
Transmit two 4-9 bit frames, or one 10-16 bit frame.
|
|
| void | USART_TxDoubleExt ( USART_TypeDef *usart, uint32_t data) |
|
Transmit two 4-9 bit frames, or one 10-16 bit frame with extended control.
|
|
| void | USART_TxExt ( USART_TypeDef *usart, uint16_t data) |
|
Transmit one 4-9 bit frame with extended control.
|
|
| void | USARTn_InitIrDA ( USART_TypeDef *usart, const USART_InitIrDA_TypeDef *init) |
|
Init USART for asynchronous IrDA mode.
|
|
Macro Definition Documentation
| #define USART_INITASYNC_DEFAULT |
Default config for USART async init structure.
Definition at line
411
of file
em_usart.h
.
Referenced by BSP_BccInit() , RETARGET_SerialInit() , and UARTDRV_InitUart() .
| #define USART_INITI2S_DEFAULT |
Default config for I2S mode init structure.
Definition at line
758
of file
em_usart.h
.
Referenced by MIC_init() .
| #define USART_INITIRDA_DEFAULT |
Default config for IrDA mode init structure.
Definition at line
667
of file
em_usart.h
.
| #define USART_INITPRSTRIGGER_DEFAULT |
Default config for USART PRS triggering structure.
Definition at line
440
of file
em_usart.h
.
| #define USART_INITSYNC_DEFAULT |
Default config for USART sync init structure.
Definition at line
522
of file
em_usart.h
.
Referenced by MICROSD_Init() , and SPIDRV_Init() .
Enumeration Type Documentation
Clock polarity/phase mode.
Definition at line
168
of file
em_usart.h
.
Databit selection.
Definition at line
104
of file
em_usart.h
.
| enum USART_Enable_TypeDef |
I2S format selection.
Definition at line
219
of file
em_usart.h
.
| enum USART_IrDAPw_Typedef |
Pulse width selection for IrDA mode.
Definition at line
183
of file
em_usart.h
.
| enum USART_OVS_TypeDef |
| enum USART_Parity_TypeDef |
Function Documentation
| void USART_BaudrateAsyncSet | ( | USART_TypeDef * |
usart,
|
| uint32_t |
refFreq,
|
||
| uint32_t |
baudrate,
|
||
| USART_OVS_TypeDef |
ovs
|
||
| ) |
Configure USART/UART operating in asynchronous mode to use a given baudrate (or as close as possible to specified baudrate).
- Parameters
-
[in] usartPointer to USART/UART peripheral register block. [in] refFreqUSART/UART reference clock frequency in Hz that will be used. If set to 0, the currently configured reference clock is assumed. [in] baudrateBaudrate to try to achieve for USART/UART. [in] ovsOversampling to be used. Normal is 16x oversampling, but lower oversampling may be used to achieve higher rates or better baudrate accuracy in some cases. Notice that lower oversampling frequency makes channel more vulnerable to bit faults during reception due to clock inaccuracies compared to link partner.
Definition at line
189
of file
em_usart.c
.
References _USART_CTRL_OVS_MASK , USART_TypeDef::CLKDIV , CMU_ClockFreqGet() , cmuClock_HFPER , USART_TypeDef::CTRL , usartOVS16 , usartOVS4 , usartOVS6 , and usartOVS8 .
Referenced by USART_InitAsync() .
| uint32_t USART_BaudrateCalc | ( | uint32_t |
refFreq,
|
| uint32_t |
clkdiv,
|
||
| bool |
syncmode,
|
||
| USART_OVS_TypeDef |
ovs
|
||
| ) |
Calculate baudrate for USART/UART given reference frequency, clock division and oversampling rate (if async mode).
This function returns the baudrate that a USART/UART module will use if configured with the given frequency, clock divisor and mode. Notice that this function will not use actual HW configuration. It can be used to determinate if a given configuration is sufficiently accurate for the application.
- Parameters
-
[in] refFreqUSART/UART HF peripheral frequency used. [in] clkdivClock division factor to be used. [in] syncmode- true - synchronous mode operation.
- false - asynchronous mode operation.
[in] ovsOversampling used if asynchronous mode. Not used if syncmodeis true.
- Returns
- Baudrate with given settings.
Definition at line
317
of file
em_usart.c
.
References usartOVS16 , usartOVS6 , and usartOVS8 .
Referenced by USART_BaudrateGet() .
| uint32_t USART_BaudrateGet | ( | USART_TypeDef * |
usart
|
) |
Get current baudrate for USART/UART.
This function returns the actual baudrate (not considering oscillator inaccuracies) used by a USART/UART peripheral.
- Parameters
-
[in] usartPointer to USART/UART peripheral register block.
- Returns
- Current baudrate.
Definition at line
448
of file
em_usart.c
.
References _USART_CTRL_OVS_MASK , USART_TypeDef::CLKDIV , CMU_ClockFreqGet() , cmuClock_HFPER , USART_TypeDef::CTRL , USART_BaudrateCalc() , and USART_CTRL_SYNC .
Referenced by SPIDRV_GetBitrate() .
| void USART_BaudrateSyncSet | ( | USART_TypeDef * |
usart,
|
| uint32_t |
refFreq,
|
||
| uint32_t |
baudrate
|
||
| ) |
Configure USART operating in synchronous mode to use a given baudrate (or as close as possible to specified baudrate).
The configuration will be set to use a baudrate <= the specified baudrate in order to ensure that the baudrate does not exceed the specified value.
Fractional clock division is suppressed, although the HW design allows it. It could cause half clock cycles to exceed specified limit, and thus potentially violate specifications for the slave device. In some special situations fractional clock division may be useful even in synchronous mode, but in those cases it must be directly adjusted, possibly assisted by USART_BaudrateCalc() :
- Parameters
-
[in] usartPointer to USART peripheral register block. (Cannot be used on UART modules.) [in] refFreqUSART reference clock frequency in Hz that will be used. If set to 0, the currently configured reference clock is assumed. [in] baudrateBaudrate to try to achieve for USART.
Definition at line
493
of file
em_usart.c
.
References USART_TypeDef::CLKDIV , CMU_ClockFreqGet() , and cmuClock_HFPER .
Referenced by MICROSD_SpiClkFast() , MICROSD_SpiClkSlow() , SPIDRV_SetBitrate() , and USART_InitSync() .
| void USART_Enable | ( | USART_TypeDef * |
usart,
|
| USART_Enable_TypeDef |
enable
|
||
| ) |
Enable/disable USART/UART receiver and/or transmitter.
Notice that this function does not do any configuration. Enabling should normally be done after initialization is done (if not enabled as part of init).
- Parameters
-
[in] usartPointer to USART/UART peripheral register block. [in] enableSelect status for receiver/transmitter.
Definition at line
535
of file
em_usart.c
.
References _USART_CMD_RXEN_MASK , _USART_CMD_TXEN_MASK , and USART_TypeDef::CMD .
Referenced by RETARGET_SerialInit() , UARTDRV_InitUart() , and USART_InitI2s() .
| void USART_InitAsync | ( | USART_TypeDef * |
usart,
|
| const USART_InitAsync_TypeDef * |
init
|
||
| ) |
Init USART/UART for normal asynchronous mode.
This function will configure basic settings in order to operate in normal asynchronous mode.
Special control setup not covered by this function must be done after using this function by direct modification of the CTRL register.
Notice that pins used by the USART/UART module must be properly configured by the user explicitly, in order for the USART/UART to work as intended. (When configuring pins, one should remember to consider the sequence of configuration, in order to avoid unintended pulses/glitches on output pins.)
- Parameters
-
[in] usartPointer to USART/UART peripheral register block. [in] initPointer to initialization structure used to configure basic async setup.
Definition at line
576
of file
em_usart.c
.
References USART_InitAsync_TypeDef::baudrate , USART_TypeDef::CMD , USART_TypeDef::CTRL , USART_InitAsync_TypeDef::databits , USART_InitAsync_TypeDef::enable , USART_TypeDef::FRAME , USART_TypeDef::INPUT , USART_InitAsync_TypeDef::mvdis , USART_InitAsync_TypeDef::oversampling , USART_InitAsync_TypeDef::parity , USART_InitAsync_TypeDef::prsRxCh , USART_InitAsync_TypeDef::prsRxEnable , USART_InitAsync_TypeDef::refFreq , USART_InitAsync_TypeDef::stopbits , USART_BaudrateAsyncSet() , USART_CTRL_AUTOCS , USART_CTRL_MVDIS , USART_INPUT_RXPRS , and USART_Reset() .
Referenced by BSP_BccInit() , RETARGET_SerialInit() , UARTDRV_InitUart() , and USARTn_InitIrDA() .
| void USART_InitI2s | ( | USART_TypeDef * |
usart,
|
| USART_InitI2s_TypeDef * |
init
|
||
| ) |
Init USART for I2S mode.
This function will configure basic settings in order to operate in I2S mode.
Special control setup not covered by this function must be done after using this function by direct modification of the CTRL and I2SCTRL registers.
Notice that pins used by the USART module must be properly configured by the user explicitly, in order for the USART to work as intended. (When configuring pins, one should remember to consider the sequence of configuration, in order to avoid unintended pulses/glitches on output pins.)
- Parameters
-
[in] usartPointer to USART peripheral register block. (UART does not support this mode.) [in] initPointer to initialization structure used to configure basic I2S setup.
- Note
- This function does not apply to all USART's. Refer to chip manuals.
Definition at line
782
of file
em_usart.c
.
References USART_InitI2s_TypeDef::delay , USART_InitI2s_TypeDef::dmaSplit , USART_InitSync_TypeDef::enable , USART_InitI2s_TypeDef::format , USART_TypeDef::I2SCTRL , USART_InitI2s_TypeDef::justify , USART_InitI2s_TypeDef::mono , USART_InitI2s_TypeDef::sync , USART_Enable() , USART_I2SCTRL_DELAY , USART_I2SCTRL_DMASPLIT , USART_I2SCTRL_EN , USART_I2SCTRL_MONO , USART_InitSync() , and usartDisable .
Referenced by MIC_init() .
| __STATIC_INLINE void USART_InitIrDA | ( | const USART_InitIrDA_TypeDef * |
init
|
) |
Init DEFAULT_IRDA_USART for asynchronous IrDA mode.
This function will configure basic settings in order to operate in asynchronous IrDA mode.
Special control setup not covered by this function must be done after using this function by direct modification of the CTRL and IRCTRL registers.
Notice that pins used by the USART/UART module must be properly configured by the user explicitly, in order for the USART/UART to work as intended. (When configuring pins, one should remember to consider the sequence of configuration, in order to avoid unintended pulses/glitches on output pins.)
- Parameters
-
[in] initPointer to initialization structure used to configure async IrDA setup.
- Deprecated:
- Deprecated function. New code should use USARTn_InitIrDA() . This function uses DEFAULT_IRDA_USART, which unless otherwise specified, is USART0 on most devices, and USART1 on devices that don't have a USART0.
Definition at line
836
of file
em_usart.h
.
References USART0 , and USARTn_InitIrDA() .
| void USART_InitPrsTrigger | ( | USART_TypeDef * |
usart,
|
| const USART_PrsTriggerInit_TypeDef * |
init
|
||
| ) |
Initialize automatic transmissions using PRS channel as trigger.
- Note
- Initialize USART with USART_Init() before setting up PRS configuration
- Parameters
-
[in] usartPointer to USART to configure [in] initPointer to initialization structure
Definition at line
819
of file
em_usart.c
.
References _USART_TRIGCTRL_AUTOTXTEN_MASK , _USART_TRIGCTRL_RXTEN_MASK , _USART_TRIGCTRL_TSEL_MASK , _USART_TRIGCTRL_TXTEN_MASK , USART_PrsTriggerInit_TypeDef::autoTxTriggerEnable , USART_PrsTriggerInit_TypeDef::prsTriggerChannel , USART_PrsTriggerInit_TypeDef::rxTriggerEnable , USART_TypeDef::TRIGCTRL , USART_PrsTriggerInit_TypeDef::txTriggerEnable , USART_TRIGCTRL_AUTOTXTEN , USART_TRIGCTRL_RXTEN , and USART_TRIGCTRL_TXTEN .
| void USART_InitSync | ( | USART_TypeDef * |
usart,
|
| const USART_InitSync_TypeDef * |
init
|
||
| ) |
Init USART for synchronous mode.
This function will configure basic settings in order to operate in synchronous mode.
Special control setup not covered by this function must be done after using this function by direct modification of the CTRL register.
Notice that pins used by the USART module must be properly configured by the user explicitly, in order for the USART to work as intended. (When configuring pins, one should remember to consider the sequence of configuration, in order to avoid unintended pulses/glitches on output pins.)
- Parameters
-
[in] usartPointer to USART peripheral register block. (UART does not support this mode.) [in] initPointer to initialization structure used to configure basic async setup.
Definition at line
649
of file
em_usart.c
.
References USART_InitSync_TypeDef::autoTx , USART_InitSync_TypeDef::baudrate , USART_InitSync_TypeDef::clockMode , USART_TypeDef::CMD , USART_TypeDef::CTRL , USART_InitSync_TypeDef::databits , USART_InitSync_TypeDef::enable , USART_TypeDef::FRAME , USART_TypeDef::INPUT , USART_InitSync_TypeDef::master , USART_InitSync_TypeDef::msbf , USART_InitSync_TypeDef::prsRxCh , USART_InitSync_TypeDef::prsRxEnable , USART_InitSync_TypeDef::refFreq , USART_BaudrateSyncSet() , USART_CMD_MASTEREN , USART_CTRL_AUTOCS , USART_CTRL_AUTOTX , USART_CTRL_MSBF , USART_CTRL_SYNC , USART_FRAME_PARITY_DEFAULT , USART_FRAME_STOPBITS_DEFAULT , USART_INPUT_RXPRS , and USART_Reset() .
Referenced by ICM20648_spiInit() , MICROSD_Init() , SPI_TFT_Init() , SPIDRV_Init() , and USART_InitI2s() .
| __STATIC_INLINE void USART_IntClear | ( | USART_TypeDef * |
usart,
|
| uint32_t |
flags
|
||
| ) |
Clear one or more pending USART interrupts.
- Parameters
-
[in] usartPointer to USART/UART peripheral register block. [in] flagsPending USART/UART interrupt source(s) to clear. Use one or more valid interrupt flags for the USART module (USART_IF_nnn) OR'ed together.
Definition at line
860
of file
em_usart.h
.
References USART_TypeDef::IFC .
Referenced by RETARGET_SerialInit() , and UARTDRV_InitUart() .
| __STATIC_INLINE void USART_IntDisable | ( | USART_TypeDef * |
usart,
|
| uint32_t |
flags
|
||
| ) |
Disable one or more USART interrupts.
- Parameters
-
[in] usartPointer to USART/UART peripheral register block. [in] flagsUSART/UART interrupt source(s) to disable. Use one or more valid interrupt flags for the USART module (USART_IF_nnn) OR'ed together.
Definition at line
876
of file
em_usart.h
.
References USART_TypeDef::IEN .
Referenced by disableRxInterrupt() .
| __STATIC_INLINE void USART_IntEnable | ( | USART_TypeDef * |
usart,
|
| uint32_t |
flags
|
||
| ) |
Enable one or more USART interrupts.
- Note
- Depending on the use, a pending interrupt may already be set prior to enabling the interrupt. Consider using USART_IntClear() prior to enabling if such a pending interrupt should be ignored.
- Parameters
-
[in] usartPointer to USART/UART peripheral register block. [in] flagsUSART/UART interrupt source(s) to enable. Use one or more valid interrupt flags for the USART module (USART_IF_nnn) OR'ed together.
Definition at line
897
of file
em_usart.h
.
References USART_TypeDef::IEN .
Referenced by enableRxInterrupt() , and RETARGET_SerialInit() .
| __STATIC_INLINE uint32_t USART_IntGet | ( | USART_TypeDef * |
usart
|
) |
Get pending USART interrupt flags.
- Note
- The event bits are not cleared by the use of this function.
- Parameters
-
[in] usartPointer to USART/UART peripheral register block.
- Returns
- USART/UART interrupt source(s) pending. Returns one or more valid interrupt flags for the USART module (USART_IF_nnn) OR'ed together.
Definition at line
916
of file
em_usart.h
.
References USART_TypeDef::IF .
| __STATIC_INLINE uint32_t USART_IntGetEnabled | ( | USART_TypeDef * |
usart
|
) |
Get enabled and pending USART interrupt flags. Useful for handling more interrupt sources in the same interrupt handler.
- Parameters
-
[in] usartPointer to USART/UART peripheral register block.
- Note
- Interrupt flags are not cleared by the use of this function.
- Returns
-
Pending and enabled USART interrupt sources. The return value is the bitwise AND combination of
- the OR combination of enabled interrupt sources in USARTx_IEN_nnn register (USARTx_IEN_nnn) and
- the OR combination of valid interrupt flags of the USART module (USARTx_IF_nnn).
Definition at line
940
of file
em_usart.h
.
References USART_TypeDef::IEN , and USART_TypeDef::IF .
| __STATIC_INLINE void USART_IntSet | ( | USART_TypeDef * |
usart,
|
| uint32_t |
flags
|
||
| ) |
Set one or more pending USART interrupts from SW.
- Parameters
-
[in] usartPointer to USART/UART peripheral register block. [in] flagsUSART/UART interrupt source(s) to set to pending. Use one or more valid interrupt flags for the USART module (USART_IF_nnn) OR'ed together.
Definition at line
963
of file
em_usart.h
.
References USART_TypeDef::IFS .
| void USART_Reset | ( | USART_TypeDef * |
usart
|
) |
Reset USART/UART to same state as after a HW reset.
- Parameters
-
[in] usartPointer to USART/UART peripheral register block.
Definition at line
855
of file
em_usart.c
.
References _USART_CLKDIV_RESETVALUE , _USART_CTRL_RESETVALUE , _USART_FRAME_RESETVALUE , _USART_I2SCTRL_RESETVALUE , _USART_IEN_RESETVALUE , _USART_IFC_MASK , _USART_INPUT_RESETVALUE , _USART_IRCTRL_RESETVALUE , _USART_ROUTE_RESETVALUE , _USART_TRIGCTRL_RESETVALUE , USART_TypeDef::CLKDIV , USART_TypeDef::CMD , USART_TypeDef::CTRL , USART_TypeDef::FRAME , USART_TypeDef::I2SCTRL , USART_TypeDef::IEN , USART_TypeDef::IFC , USART_TypeDef::INPUT , USART_TypeDef::IRCTRL , USART_TypeDef::ROUTE , USART_TypeDef::TRIGCTRL , USART_CMD_CLEARRX , USART_CMD_CLEARTX , USART_CMD_MASTERDIS , USART_CMD_RXBLOCKDIS , USART_CMD_RXDIS , USART_CMD_TXDIS , and USART_CMD_TXTRIDIS .
Referenced by BOARD_flashDeepPowerDown() , BSP_BccDeInit() , ICM20648_spiInit() , MIC_deInit() , MICROSD_Deinit() , SPI_TFT_Init() , SPIDRV_DeInit() , USART_InitAsync() , and USART_InitSync() .
| uint8_t USART_Rx | ( | USART_TypeDef * |
usart
|
) |
Receive one 4-8 bit frame, (or part of 10-16 bit frame).
This function is normally used to receive one frame when operating with frame length 4-8 bits. Please refer to USART_RxExt() for reception of 9 bit frames.
Notice that possible parity/stop bits in asynchronous mode are not considered part of specified frame bit length.
- Note
- This function will stall if the buffer is empty, until data is received. Alternatively the user can explicitly check whether data is available, and if data is avaliable, call USART_RxDataGet() to read the RXDATA register directly.
- Parameters
-
[in] usartPointer to USART/UART peripheral register block.
- Returns
- Data received.
Definition at line
919
of file
em_usart.c
.
References USART_TypeDef::RXDATA , USART_TypeDef::STATUS , and USART_STATUS_RXDATAV .
Referenced by ICM20648_bankSelect() , ICM20648_registerRead() , ICM20648_registerWrite() , and SPI_TFT_WriteRegister() .
| __STATIC_INLINE uint8_t USART_RxDataGet | ( | USART_TypeDef * |
usart
|
) |
Receive one 4-8 bit frame, (or part of 10-16 bit frame).
This function is used to quickly receive one 4-8 bits frame by reading the RXDATA register directly, without checking the STATUS register for the RXDATAV flag. This can be useful from the RXDATAV interrupt handler, i.e. waiting is superfluous, in order to quickly read the received data. Please refer to USART_RxDataXGet() for reception of 9 bit frames.
- Note
- Since this function does not check whether the RXDATA register actually holds valid data, it should only be used in situations when it is certain that there is valid data, ensured by some external program routine, e.g. like when handling an RXDATAV interrupt. The USART_Rx() is normally a better choice if the validity of the RXDATA register is not certain.
- Notice that possible parity/stop bits in asynchronous mode are not considered part of specified frame bit length.
- Parameters
-
[in] usartPointer to USART/UART peripheral register block.
- Returns
- Data received.
Definition at line
1018
of file
em_usart.h
.
References USART_TypeDef::RXDATA .
| __STATIC_INLINE uint16_t USART_RxDataXGet | ( | USART_TypeDef * |
usart
|
) |
Receive one 4-9 bit frame, (or part of 10-16 bit frame) with extended information.
This function is used to quickly receive one 4-9 bit frame, (or part of 10-16 bit frame) with extended information by reading the RXDATAX register directly, without checking the STATUS register for the RXDATAV flag. This can be useful from the RXDATAV interrupt handler, i.e. waiting is superfluous, in order to quickly read the received data.
- Note
- Since this function does not check whether the RXDATAX register actually holds valid data, it should only be used in situations when it is certain that there is valid data, ensured by some external program routine, e.g. like when handling an RXDATAV interrupt. The USART_RxExt() is normally a better choice if the validity of the RXDATAX register is not certain.
- Notice that possible parity/stop bits in asynchronous mode are not considered part of specified frame bit length.
- Parameters
-
[in] usartPointer to USART/UART peripheral register block.
- Returns
- Data received.
Definition at line
1124
of file
em_usart.h
.
References USART_TypeDef::RXDATAX .
| uint16_t USART_RxDouble | ( | USART_TypeDef * |
usart
|
) |
Receive two 4-8 bit frames, or one 10-16 bit frame.
This function is normally used to receive one frame when operating with frame length 10-16 bits. Please refer to USART_RxDoubleExt() for reception of two 9 bit frames.
Notice that possible parity/stop bits in asynchronous mode are not considered part of specified frame bit length.
- Note
- This function will stall if buffer is empty, until data is received. Alternatively the user can explicitly check whether data is available, and if data is avaliable, call USART_RxDoubleGet() to read the RXDOUBLE register directly.
- Parameters
-
[in] usartPointer to USART/UART peripheral register block.
- Returns
- Data received.
Definition at line
951
of file
em_usart.c
.
References USART_TypeDef::RXDOUBLE , USART_TypeDef::STATUS , and USART_STATUS_RXFULL .
| uint32_t USART_RxDoubleExt | ( | USART_TypeDef * |
usart
|
) |
Receive two 4-9 bit frames, or one 10-16 bit frame with extended information.
This function is normally used to receive one frame when operating with frame length 10-16 bits and additional RX status information is required.
Notice that possible parity/stop bits in asynchronous mode are not considered part of specified frame bit length.
- Note
- This function will stall if buffer is empty, until data is received. Alternatively the user can explicitly check whether data is available, and if data is avaliable, call USART_RxDoubleXGet() to read the RXDOUBLEX register directly.
- Parameters
-
[in] usartPointer to USART/UART peripheral register block.
- Returns
- Data received.
Definition at line
983
of file
em_usart.c
.
References USART_TypeDef::RXDOUBLEX , USART_TypeDef::STATUS , and USART_STATUS_RXFULL .
| __STATIC_INLINE uint16_t USART_RxDoubleGet | ( | USART_TypeDef * |
usart
|
) |
Receive two 4-8 bit frames, or one 10-16 bit frame.
This function is used to quickly receive one 10-16 bits frame or two 4-8 bit frames by reading the RXDOUBLE register directly, without checking the STATUS register for the RXDATAV flag. This can be useful from the RXDATAV interrupt handler, i.e. waiting is superfluous, in order to quickly read the received data. This function is normally used to receive one frame when operating with frame length 10-16 bits. Please refer to USART_RxDoubleXGet() for reception of two 9 bit frames.
- Note
- Since this function does not check whether the RXDOUBLE register actually holds valid data, it should only be used in situations when it is certain that there is valid data, ensured by some external program routine, e.g. like when handling an RXDATAV interrupt. The USART_RxDouble() is normally a better choice if the validity of the RXDOUBLE register is not certain.
- Notice that possible parity/stop bits in asynchronous mode are not considered part of specified frame bit length.
- Parameters
-
[in] usartPointer to USART/UART peripheral register block.
- Returns
- Data received.
Definition at line
1055
of file
em_usart.h
.
References USART_TypeDef::RXDOUBLE .
| __STATIC_INLINE uint32_t USART_RxDoubleXGet | ( | USART_TypeDef * |
usart
|
) |
Receive two 4-9 bit frames, or one 10-16 bit frame with extended information.
This function is used to quickly receive one 10-16 bits frame or two 4-9 bit frames by reading the RXDOUBLEX register directly, without checking the STATUS register for the RXDATAV flag. This can be useful from the RXDATAV interrupt handler, i.e. waiting is superfluous, in order to quickly read the received data.
- Note
- Since this function does not check whether the RXDOUBLEX register actually holds valid data, it should only be used in situations when it is certain that there is valid data, ensured by some external program routine, e.g. like when handling an RXDATAV interrupt. The USART_RxDoubleExt() is normally a better choice if the validity of the RXDOUBLEX register is not certain.
- Notice that possible parity/stop bits in asynchronous mode are not considered part of specified frame bit length.
- Parameters
-
[in] usartPointer to USART/UART peripheral register block.
- Returns
- Data received.
Definition at line
1090
of file
em_usart.h
.
References USART_TypeDef::RXDOUBLEX .
| uint16_t USART_RxExt | ( | USART_TypeDef * |
usart
|
) |
Receive one 4-9 bit frame, (or part of 10-16 bit frame) with extended information.
This function is normally used to receive one frame when operating with frame length 4-9 bits and additional RX status information is required.
Notice that possible parity/stop bits in asynchronous mode are not considered part of specified frame bit length.
- Note
- This function will stall if buffer is empty, until data is received. Alternatively the user can explicitly check whether data is available, and if data is avaliable, call USART_RxDataXGet() to read the RXDATAX register directly.
- Parameters
-
[in] usartPointer to USART/UART peripheral register block.
- Returns
- Data received.
Definition at line
1015
of file
em_usart.c
.
References USART_TypeDef::RXDATAX , USART_TypeDef::STATUS , and USART_STATUS_RXDATAV .
| uint8_t USART_SpiTransfer | ( | USART_TypeDef * |
usart,
|
| uint8_t |
data
|
||
| ) |
Perform one 8 bit frame SPI transfer.
- Note
- This function will stall if the transmit buffer is full. When a transmit buffer becomes available, data is written and the function will wait until the data is fully transmitted. The SPI return value is then read out and returned.
- Parameters
-
[in] usartPointer to USART peripheral register block. [in] dataData to transmit.
- Returns
- Data received.
Definition at line
1042
of file
em_usart.c
.
References USART_TypeDef::RXDATA , USART_TypeDef::STATUS , USART_TypeDef::TXDATA , USART_STATUS_TXBL , and USART_STATUS_TXC .
Referenced by BOARD_flashDeepPowerDown() , and MICROSD_XferSpi() .
| __STATIC_INLINE uint32_t USART_StatusGet | ( | USART_TypeDef * |
usart
|
) |
Get USART STATUS register.
- Parameters
-
[in] usartPointer to USART/UART peripheral register block.
- Returns
- STATUS register value.
Definition at line
979
of file
em_usart.h
.
References USART_TypeDef::STATUS .
| void USART_Tx | ( | USART_TypeDef * |
usart,
|
| uint8_t |
data
|
||
| ) |
Transmit one 4-9 bit frame.
Depending on frame length configuration, 4-8 (least significant) bits from
data
are transmitted. If frame length is 9, 8 bits are transmitted from
data
and one bit as specified by CTRL register, BIT8DV field. Please refer to
USART_TxExt()
for transmitting 9 bit frame with full control of all 9 bits.
Notice that possible parity/stop bits in asynchronous mode are not considered part of specified frame bit length.
- Note
- This function will stall if buffer is full, until buffer becomes available.
- Parameters
-
[in] usartPointer to USART/UART peripheral register block. [in] dataData to transmit. See details above for further info.
Definition at line
1075
of file
em_usart.c
.
References USART_TypeDef::STATUS , USART_TypeDef::TXDATA , and USART_STATUS_TXBL .
Referenced by ICM20648_bankSelect() , ICM20648_registerRead() , ICM20648_registerWrite() , SPI_TFT_WriteRegister() , and UARTDRV_ForceTransmit() .
| void USART_TxDouble | ( | USART_TypeDef * |
usart,
|
| uint16_t |
data
|
||
| ) |
Transmit two 4-9 bit frames, or one 10-16 bit frame.
Depending on frame length configuration, 4-8 (least significant) bits from each byte in
data
are transmitted. If frame length is 9, 8 bits are transmitted from each byte in
data
adding one bit as specified by CTRL register, BIT8DV field, to each byte. Please refer to
USART_TxDoubleExt()
for transmitting two 9 bit frames with full control of all 9 bits.
If frame length is 10-16, 10-16 (least significant) bits from
data
are transmitted.
Notice that possible parity/stop bits in asynchronous mode are not considered part of specified frame bit length.
- Note
- This function will stall if buffer is full, until buffer becomes available.
- Parameters
-
[in] usartPointer to USART/UART peripheral register block. [in] dataData to transmit, the least significant byte holds the frame transmitted first. See details above for further info.
Definition at line
1110
of file
em_usart.c
.
References USART_TypeDef::STATUS , USART_TypeDef::TXDOUBLE , and USART_STATUS_TXBL .
| void USART_TxDoubleExt | ( | USART_TypeDef * |
usart,
|
| uint32_t |
data
|
||
| ) |
Transmit two 4-9 bit frames, or one 10-16 bit frame with extended control.
Notice that possible parity/stop bits in asynchronous mode are not considered part of specified frame bit length.
- Note
- This function will stall if buffer is full, until buffer becomes available.
- Parameters
-
[in] usartPointer to USART/UART peripheral register block. [in] dataData to transmit with extended control. Contains two 16 bit words concatenated. Least significant word holds frame transitted first. If frame length is 4-9, two frames with 4-9 least significant bits from each 16 bit word are transmitted.
- If frame length is 10-16 bits, 8 data bits are taken from the least significant 16 bit word, and the remaining bits from the other 16 bit word.
- Additional control bits are available as documented in the reference manual (set to 0 if not used). For 10-16 bit frame length, these control bits are taken from the most significant 16 bit word.
Definition at line
1145
of file
em_usart.c
.
References USART_TypeDef::STATUS , USART_TypeDef::TXDOUBLEX , and USART_STATUS_TXBL .
| void USART_TxExt | ( | USART_TypeDef * |
usart,
|
| uint16_t |
data
|
||
| ) |
Transmit one 4-9 bit frame with extended control.
Notice that possible parity/stop bits in asynchronous mode are not considered part of specified frame bit length.
- Note
- This function will stall if buffer is full, until buffer becomes available.
- Parameters
-
[in] usartPointer to USART/UART peripheral register block. [in] dataData to transmit with extended control. Least significant bits contains frame bits, and additional control bits are available as documented in the reference manual (set to 0 if not used).
Definition at line
1172
of file
em_usart.c
.
References USART_TypeDef::STATUS , USART_TypeDef::TXDATAX , and USART_STATUS_TXBL .
| void USARTn_InitIrDA | ( | USART_TypeDef * |
usart,
|
| const USART_InitIrDA_TypeDef * |
init
|
||
| ) |
Init USART for asynchronous IrDA mode.
This function will configure basic settings in order to operate in asynchronous IrDA mode.
Special control setup not covered by this function must be done after using this function by direct modification of the CTRL and IRCTRL registers.
Notice that pins used by the USART/UART module must be properly configured by the user explicitly, in order for the USART/UART to work as intended. (When configuring pins, one should remember to consider the sequence of configuration, in order to avoid unintended pulses/glitches on output pins.)
- Parameters
-
[in] usartPointer to USART peripheral register block. [in] initPointer to initialization structure used to configure async IrDA setup.
- Note
- Not all USART instances support IrDA. See the datasheet for your device.
Definition at line
727
of file
em_usart.c
.
References _USART_IRCTRL_IRFILT_SHIFT , _USART_IRCTRL_IRPRSEN_SHIFT , USART_InitIrDA_TypeDef::async , USART_TypeDef::CTRL , USART_TypeDef::IRCTRL , USART_InitIrDA_TypeDef::irFilt , USART_InitIrDA_TypeDef::irPrsEn , USART_InitIrDA_TypeDef::irPrsSel , USART_InitIrDA_TypeDef::irPw , USART_InitIrDA_TypeDef::irRxInv , USART_CTRL_RXINV , USART_CTRL_TXINV , USART_InitAsync() , and USART_IRCTRL_IREN .
Referenced by USART_InitIrDA() .