DMA_CfgDescr_TypeDef Struct ReferenceEMLIB > DMA
Configuration structure for primary or alternate descriptor (not used for scatter-gather DMA cycles).
       Definition at line
       
        203
       
       of file
       
        em_dma.h
       
       .
      
      
       #include <
       
     
        em_dma.h
       
       >
      
         Data Fields | 
       |
| DMA_ArbiterConfig_TypeDef | arbRate | 
| DMA_DataInc_TypeDef | dstInc | 
| uint8_t | hprot | 
| DMA_DataSize_TypeDef | size | 
| DMA_DataInc_TypeDef | srcInc | 
Field Documentation
| DMA_ArbiterConfig_TypeDef DMA_CfgDescr_TypeDef::arbRate | 
Arbitration rate, ie number of DMA transfers done before rearbitration takes place.
        Definition at line
        
         217
        
        of file
        
         em_dma.h
        
        .
       
Referenced by DMA_CfgDescr() .
| DMA_DataInc_TypeDef DMA_CfgDescr_TypeDef::dstInc | 
Destination increment size for each DMA transfer
        Definition at line
        
         205
        
        of file
        
         em_dma.h
        
        .
       
Referenced by DMA_CfgDescr() .
| uint8_t DMA_CfgDescr_TypeDef::hprot | 
HPROT signal state, please refer to reference manual, DMA chapter for further details. Normally set to 0 if protection is not an issue. The following bits are available:
- bit 0 - HPROT[1] control for source read accesses, privileged/non-privileged access
 - bit 3 - HPROT[1] control for destination write accesses, privileged/non-privileged access
 
        Definition at line
        
         228
        
        of file
        
         em_dma.h
        
        .
       
Referenced by DMA_CfgDescr() .
| DMA_DataSize_TypeDef DMA_CfgDescr_TypeDef::size | 
| DMA_DataInc_TypeDef DMA_CfgDescr_TypeDef::srcInc | 
Source increment size for each DMA transfer
        Definition at line
        
         208
        
        of file
        
         em_dma.h
        
        .
       
Referenced by DMA_CfgDescr() .
The documentation for this struct was generated from the following file:
- 
       C:/repos/embsw_super_h1/platform/emlib/inc/
       
em_dma.h