USB_StringDescriptor_TypeDef Struct ReferencePlatform Middleware > USB > USB_COMMON
USB String Descriptor.
       Definition at line
       
        496
       
       of file
       
        em_usb.h
       
       .
      
      
       #include <
       
     
        em_usb.h
       
       >
      
         Data Fields | 
       |
| uint8_t | len | 
| char16_t | name [] | 
| uint8_t | type | 
Field Documentation
| uint8_t USB_StringDescriptor_TypeDef::len | 
Size of this descriptor in bytes.
        Definition at line
        
         497
        
        of file
        
         em_usb.h
        
        .
       
| char16_t USB_StringDescriptor_TypeDef::name[] | 
The string encoded with UTF-16LE UNICODE charset.
        Definition at line
        
         499
        
        of file
        
         em_usb.h
        
        .
       
| uint8_t USB_StringDescriptor_TypeDef::type | 
Constant STRING Descriptor Type.
        Definition at line
        
         498
        
        of file
        
         em_usb.h
        
        .
       
The documentation for this struct was generated from the following file:
- 
       C:/repos/embsw_super_h1/platform/middleware/usb_gecko/inc/
       
em_usb.h