CMU_TypeDef Struct ReferenceDevices > EZR32HG_CMU
       Definition at line
       
        48
       
       of file
       
        ezr32hg_cmu.h
       
       .
      
         Data Fields | 
       |
| __IOM uint32_t | AUXHFRCOCTRL | 
| __IOM uint32_t | CALCNT | 
| __IOM uint32_t | CALCTRL | 
| __IOM uint32_t | CMD | 
| __IOM uint32_t | CTRL | 
| __IOM uint32_t | FREEZE | 
| __IOM uint32_t | HFCORECLKDIV | 
| __IOM uint32_t | HFCORECLKEN0 | 
| __IOM uint32_t | HFPERCLKDIV | 
| __IOM uint32_t | HFPERCLKEN0 | 
| __IOM uint32_t | HFRCOCTRL | 
| __IOM uint32_t | IEN | 
| __IM uint32_t | IF | 
| __IOM uint32_t | IFC | 
| __IOM uint32_t | IFS | 
| __IOM uint32_t | LFACLKEN0 | 
| __IOM uint32_t | LFAPRESC0 | 
| __IOM uint32_t | LFBCLKEN0 | 
| __IOM uint32_t | LFBPRESC0 | 
| __IOM uint32_t | LFCCLKEN0 | 
| __IOM uint32_t | LFCLKSEL | 
| __IOM uint32_t | LFRCOCTRL | 
| __IOM uint32_t | LOCK | 
| __IOM uint32_t | OSCENCMD | 
| __IOM uint32_t | PCNTCTRL | 
| uint32_t | RESERVED0 [2] | 
| uint32_t | RESERVED1 [1] | 
| uint32_t | RESERVED2 [1] | 
| uint32_t | RESERVED3 [1] | 
| uint32_t | RESERVED4 [1] | 
| uint32_t | RESERVED5 [18] | 
| __IOM uint32_t | ROUTE | 
| __IM uint32_t | STATUS | 
| __IM uint32_t | SYNCBUSY | 
| __IOM uint32_t | USBCRCTRL | 
| __IOM uint32_t | USHFRCOCONF | 
| __IOM uint32_t | USHFRCOCTRL | 
| __IOM uint32_t | USHFRCOTUNE | 
Field Documentation
| __IOM uint32_t CMU_TypeDef::AUXHFRCOCTRL | 
AUXHFRCO Control Register
        Definition at line
        
         54
        
        of file
        
         ezr32hg_cmu.h
        
        .
       
| __IOM uint32_t CMU_TypeDef::CALCNT | 
Calibration Counter Register
        Definition at line
        
         56
        
        of file
        
         ezr32hg_cmu.h
        
        .
       
| __IOM uint32_t CMU_TypeDef::CALCTRL | 
Calibration Control Register
        Definition at line
        
         55
        
        of file
        
         ezr32hg_cmu.h
        
        .
       
| __IOM uint32_t CMU_TypeDef::CMD | 
Command Register
        Definition at line
        
         58
        
        of file
        
         ezr32hg_cmu.h
        
        .
       
| __IOM uint32_t CMU_TypeDef::CTRL | 
CMU Control Register
        Definition at line
        
         49
        
        of file
        
         ezr32hg_cmu.h
        
        .
       
| __IOM uint32_t CMU_TypeDef::FREEZE | 
Freeze Register
        Definition at line
        
         69
        
        of file
        
         ezr32hg_cmu.h
        
        .
       
| __IOM uint32_t CMU_TypeDef::HFCORECLKDIV | 
High Frequency Core Clock Division Register
        Definition at line
        
         50
        
        of file
        
         ezr32hg_cmu.h
        
        .
       
| __IOM uint32_t CMU_TypeDef::HFCORECLKEN0 | 
High Frequency Core Clock Enable Register 0
        Definition at line
        
         65
        
        of file
        
         ezr32hg_cmu.h
        
        .
       
| __IOM uint32_t CMU_TypeDef::HFPERCLKDIV | 
High Frequency Peripheral Clock Division Register
        Definition at line
        
         51
        
        of file
        
         ezr32hg_cmu.h
        
        .
       
| __IOM uint32_t CMU_TypeDef::HFPERCLKEN0 | 
High Frequency Peripheral Clock Enable Register 0
        Definition at line
        
         66
        
        of file
        
         ezr32hg_cmu.h
        
        .
       
| __IOM uint32_t CMU_TypeDef::HFRCOCTRL | 
HFRCO Control Register
        Definition at line
        
         52
        
        of file
        
         ezr32hg_cmu.h
        
        .
       
| __IOM uint32_t CMU_TypeDef::IEN | 
Interrupt Enable Register
        Definition at line
        
         64
        
        of file
        
         ezr32hg_cmu.h
        
        .
       
| __IM uint32_t CMU_TypeDef::IF | 
Interrupt Flag Register
        Definition at line
        
         61
        
        of file
        
         ezr32hg_cmu.h
        
        .
       
| __IOM uint32_t CMU_TypeDef::IFC | 
Interrupt Flag Clear Register
        Definition at line
        
         63
        
        of file
        
         ezr32hg_cmu.h
        
        .
       
| __IOM uint32_t CMU_TypeDef::IFS | 
Interrupt Flag Set Register
        Definition at line
        
         62
        
        of file
        
         ezr32hg_cmu.h
        
        .
       
| __IOM uint32_t CMU_TypeDef::LFACLKEN0 | 
Low Frequency A Clock Enable Register 0 (Async Reg)
        Definition at line
        
         70
        
        of file
        
         ezr32hg_cmu.h
        
        .
       
| __IOM uint32_t CMU_TypeDef::LFAPRESC0 | 
Low Frequency A Prescaler Register 0 (Async Reg)
        Definition at line
        
         74
        
        of file
        
         ezr32hg_cmu.h
        
        .
       
| __IOM uint32_t CMU_TypeDef::LFBCLKEN0 | 
Low Frequency B Clock Enable Register 0 (Async Reg)
        Definition at line
        
         72
        
        of file
        
         ezr32hg_cmu.h
        
        .
       
| __IOM uint32_t CMU_TypeDef::LFBPRESC0 | 
Low Frequency B Prescaler Register 0 (Async Reg)
        Definition at line
        
         76
        
        of file
        
         ezr32hg_cmu.h
        
        .
       
| __IOM uint32_t CMU_TypeDef::LFCCLKEN0 | 
Low Frequency C Clock Enable Register 0 (Async Reg)
        Definition at line
        
         73
        
        of file
        
         ezr32hg_cmu.h
        
        .
       
| __IOM uint32_t CMU_TypeDef::LFCLKSEL | 
Low Frequency Clock Select Register
        Definition at line
        
         59
        
        of file
        
         ezr32hg_cmu.h
        
        .
       
| __IOM uint32_t CMU_TypeDef::LFRCOCTRL | 
LFRCO Control Register
        Definition at line
        
         53
        
        of file
        
         ezr32hg_cmu.h
        
        .
       
| __IOM uint32_t CMU_TypeDef::LOCK | 
Configuration Lock Register
        Definition at line
        
         82
        
        of file
        
         ezr32hg_cmu.h
        
        .
       
| __IOM uint32_t CMU_TypeDef::OSCENCMD | 
Oscillator Enable/Disable Command Register
        Definition at line
        
         57
        
        of file
        
         ezr32hg_cmu.h
        
        .
       
| __IOM uint32_t CMU_TypeDef::PCNTCTRL | 
PCNT Control Register
        Definition at line
        
         78
        
        of file
        
         ezr32hg_cmu.h
        
        .
       
| uint32_t CMU_TypeDef::RESERVED0[2] | 
Reserved for future use
        Definition at line
        
         67
        
        of file
        
         ezr32hg_cmu.h
        
        .
       
| uint32_t CMU_TypeDef::RESERVED1[1] | 
Reserved for future use
        Definition at line
        
         71
        
        of file
        
         ezr32hg_cmu.h
        
        .
       
| uint32_t CMU_TypeDef::RESERVED2[1] | 
Reserved for future use
        Definition at line
        
         75
        
        of file
        
         ezr32hg_cmu.h
        
        .
       
| uint32_t CMU_TypeDef::RESERVED3[1] | 
Reserved for future use
        Definition at line
        
         77
        
        of file
        
         ezr32hg_cmu.h
        
        .
       
| uint32_t CMU_TypeDef::RESERVED4[1] | 
Reserved for future use
        Definition at line
        
         80
        
        of file
        
         ezr32hg_cmu.h
        
        .
       
| uint32_t CMU_TypeDef::RESERVED5[18] | 
Reserved for future use
        Definition at line
        
         84
        
        of file
        
         ezr32hg_cmu.h
        
        .
       
| __IOM uint32_t CMU_TypeDef::ROUTE | 
I/O Routing Register
        Definition at line
        
         81
        
        of file
        
         ezr32hg_cmu.h
        
        .
       
| __IM uint32_t CMU_TypeDef::STATUS | 
Status Register
        Definition at line
        
         60
        
        of file
        
         ezr32hg_cmu.h
        
        .
       
| __IM uint32_t CMU_TypeDef::SYNCBUSY | 
Synchronization Busy Register
        Definition at line
        
         68
        
        of file
        
         ezr32hg_cmu.h
        
        .
       
| __IOM uint32_t CMU_TypeDef::USBCRCTRL | 
USB Clock Recovery Control
        Definition at line
        
         85
        
        of file
        
         ezr32hg_cmu.h
        
        .
       
| __IOM uint32_t CMU_TypeDef::USHFRCOCONF | 
USHFRCO Configuration
        Definition at line
        
         88
        
        of file
        
         ezr32hg_cmu.h
        
        .
       
| __IOM uint32_t CMU_TypeDef::USHFRCOCTRL | 
USHFRCO Control
        Definition at line
        
         86
        
        of file
        
         ezr32hg_cmu.h
        
        .
       
| __IOM uint32_t CMU_TypeDef::USHFRCOTUNE | 
USHFRCO Frequency Tune
        Definition at line
        
         87
        
        of file
        
         ezr32hg_cmu.h
        
        .
       
The documentation for this struct was generated from the following file:
- 
       C:/repos/embsw_super_h1/platform/Device/SiliconLabs/EZR32HG/Include/
       
ezr32hg_cmu.h