MTB_TypeDef Struct ReferenceDevices > EZR32HG_MTB
       Definition at line
       
        48
       
       of file
       
        ezr32hg_mtb.h
       
       .
      
         Data Fields | 
       |
| __IOM uint32_t | BASE | 
| __IOM uint32_t | FLOW | 
| __IOM uint32_t | MASTER | 
| __IOM uint32_t | POSITION | 
Field Documentation
| __IOM uint32_t MTB_TypeDef::BASE | 
MTB Trace Base Register
        Definition at line
        
         52
        
        of file
        
         ezr32hg_mtb.h
        
        .
       
| __IOM uint32_t MTB_TypeDef::FLOW | 
MTB Trace Flow Register
        Definition at line
        
         51
        
        of file
        
         ezr32hg_mtb.h
        
        .
       
| __IOM uint32_t MTB_TypeDef::MASTER | 
MTB Trace Control Register
        Definition at line
        
         50
        
        of file
        
         ezr32hg_mtb.h
        
        .
       
| __IOM uint32_t MTB_TypeDef::POSITION | 
MTB Trace Position Register.
        Definition at line
        
         49
        
        of file
        
         ezr32hg_mtb.h
        
        .
       
The documentation for this struct was generated from the following file:
- 
       C:/repos/embsw_super_h1/platform/Device/SiliconLabs/EZR32HG/Include/
       
ezr32hg_mtb.h