ADC_InitScan_TypeDef Struct ReferenceEMLIB > ADC
Scan sequence init structure.
       Definition at line
       
        862
       
       of file
       
        em_adc.h
       
       .
      
      
       #include <
       
     
        em_adc.h
       
       >
      
         Data Fields | 
       |
| ADC_AcqTime_TypeDef | acqTime | 
| bool | diff | 
| uint32_t | input | 
| bool | leftAdjust | 
| bool | prsEnable | 
| ADC_PRSSEL_TypeDef | prsSel | 
| ADC_Ref_TypeDef | reference | 
| bool | rep | 
| ADC_Res_TypeDef | resolution | 
Field Documentation
| ADC_AcqTime_TypeDef ADC_InitScan_TypeDef::acqTime | 
Acquisition time (in ADC clock cycles).
        Definition at line
        
         870
        
        of file
        
         em_adc.h
        
        .
       
Referenced by ADC_InitScan() .
| bool ADC_InitScan_TypeDef::diff | 
Select if single ended or differential input.
        Definition at line
        
         900
        
        of file
        
         em_adc.h
        
        .
       
Referenced by ADC_InitScan() .
| uint32_t ADC_InitScan_TypeDef::input | 
        Scan input selection. If single ended (
        
         diff
        
        is false), use logical combination of ADC_SCANCTRL_INPUTMASK_CHx defines. If differential input (
        
         diff
        
        is true), use logical combination of ADC_SCANCTRL_INPUTMASK_CHxCHy defines. (Notice underscore prefix for defines used.)
       
        Definition at line
        
         888
        
        of file
        
         em_adc.h
        
        .
       
Referenced by ADC_InitScan() .
| bool ADC_InitScan_TypeDef::leftAdjust | 
Select if left adjustment should be done.
        Definition at line
        
         906
        
        of file
        
         em_adc.h
        
        .
       
Referenced by ADC_InitScan() .
| bool ADC_InitScan_TypeDef::prsEnable | 
Peripheral reflex system trigger enable.
        Definition at line
        
         903
        
        of file
        
         em_adc.h
        
        .
       
Referenced by ADC_InitScan() , and MIC_init() .
| ADC_PRSSEL_TypeDef ADC_InitScan_TypeDef::prsSel | 
        Peripheral reflex system trigger selection. Only applicable if
        
         prsEnable
        
        is enabled.
       
        Definition at line
        
         867
        
        of file
        
         em_adc.h
        
        .
       
Referenced by ADC_InitScan() , and MIC_init() .
| ADC_Ref_TypeDef ADC_InitScan_TypeDef::reference | 
Sample reference selection. Notice that for external references, the ADC calibration register must be set explicitly.
        Definition at line
        
         876
        
        of file
        
         em_adc.h
        
        .
       
Referenced by ADC_InitScan() , and MIC_init() .
| bool ADC_InitScan_TypeDef::rep | 
Select if continuous conversion until explicit stop.
        Definition at line
        
         909
        
        of file
        
         em_adc.h
        
        .
       
Referenced by ADC_InitScan() .
| ADC_Res_TypeDef ADC_InitScan_TypeDef::resolution | 
The documentation for this struct was generated from the following file:
- 
       C:/repos/embsw_super_h1/platform/emlib/inc/
       
em_adc.h