GPIO_TypeDef Struct ReferenceDevices > EZR32HG_GPIO
       Definition at line
       
        48
       
       of file
       
        ezr32hg_gpio.h
       
       .
      
         Data Fields | 
       |
| __IOM uint32_t | CMD | 
| __IOM uint32_t | CTRL | 
| __IM uint32_t | EM4WUCAUSE | 
| __IOM uint32_t | EM4WUEN | 
| __IOM uint32_t | EM4WUPOL | 
| __IOM uint32_t | EXTIFALL | 
| __IOM uint32_t | EXTIPSELH | 
| __IOM uint32_t | EXTIPSELL | 
| __IOM uint32_t | EXTIRISE | 
| __IOM uint32_t | IEN | 
| __IM uint32_t | IF | 
| __IOM uint32_t | IFC | 
| __IOM uint32_t | IFS | 
| __IOM uint32_t | INSENSE | 
| __IOM uint32_t | LOCK | 
| GPIO_P_TypeDef | P [6] | 
| uint32_t | RESERVED0 [10] | 
| __IOM uint32_t | ROUTE | 
Field Documentation
| __IOM uint32_t GPIO_TypeDef::CMD | 
GPIO Command Register
        Definition at line
        
         65
        
        of file
        
         ezr32hg_gpio.h
        
        .
       
| __IOM uint32_t GPIO_TypeDef::CTRL | 
GPIO Control Register
        Definition at line
        
         64
        
        of file
        
         ezr32hg_gpio.h
        
        .
       
| __IM uint32_t GPIO_TypeDef::EM4WUCAUSE | 
EM4 Wake-up Cause Register
        Definition at line
        
         68
        
        of file
        
         ezr32hg_gpio.h
        
        .
       
| __IOM uint32_t GPIO_TypeDef::EM4WUEN | 
EM4 Wake-up Enable Register
        Definition at line
        
         66
        
        of file
        
         ezr32hg_gpio.h
        
        .
       
| __IOM uint32_t GPIO_TypeDef::EM4WUPOL | 
EM4 Wake-up Polarity Register
        Definition at line
        
         67
        
        of file
        
         ezr32hg_gpio.h
        
        .
       
| __IOM uint32_t GPIO_TypeDef::EXTIFALL | 
External Interrupt Falling Edge Trigger Register
        Definition at line
        
         55
        
        of file
        
         ezr32hg_gpio.h
        
        .
       
| __IOM uint32_t GPIO_TypeDef::EXTIPSELH | 
External Interrupt Port Select High Register
        Definition at line
        
         53
        
        of file
        
         ezr32hg_gpio.h
        
        .
       
| __IOM uint32_t GPIO_TypeDef::EXTIPSELL | 
External Interrupt Port Select Low Register
        Definition at line
        
         52
        
        of file
        
         ezr32hg_gpio.h
        
        .
       
| __IOM uint32_t GPIO_TypeDef::EXTIRISE | 
External Interrupt Rising Edge Trigger Register
        Definition at line
        
         54
        
        of file
        
         ezr32hg_gpio.h
        
        .
       
| __IOM uint32_t GPIO_TypeDef::IEN | 
Interrupt Enable Register
        Definition at line
        
         56
        
        of file
        
         ezr32hg_gpio.h
        
        .
       
| __IM uint32_t GPIO_TypeDef::IF | 
Interrupt Flag Register
        Definition at line
        
         57
        
        of file
        
         ezr32hg_gpio.h
        
        .
       
| __IOM uint32_t GPIO_TypeDef::IFC | 
Interrupt Flag Clear Register
        Definition at line
        
         59
        
        of file
        
         ezr32hg_gpio.h
        
        .
       
| __IOM uint32_t GPIO_TypeDef::IFS | 
Interrupt Flag Set Register
        Definition at line
        
         58
        
        of file
        
         ezr32hg_gpio.h
        
        .
       
| __IOM uint32_t GPIO_TypeDef::INSENSE | 
Input Sense Register
        Definition at line
        
         62
        
        of file
        
         ezr32hg_gpio.h
        
        .
       
| __IOM uint32_t GPIO_TypeDef::LOCK | 
Configuration Lock Register
        Definition at line
        
         63
        
        of file
        
         ezr32hg_gpio.h
        
        .
       
| GPIO_P_TypeDef GPIO_TypeDef::P[6] | 
Port configuration bits
        Definition at line
        
         49
        
        of file
        
         ezr32hg_gpio.h
        
        .
       
| uint32_t GPIO_TypeDef::RESERVED0[10] | 
Reserved for future use
        Definition at line
        
         51
        
        of file
        
         ezr32hg_gpio.h
        
        .
       
| __IOM uint32_t GPIO_TypeDef::ROUTE | 
I/O Routing Register
        Definition at line
        
         61
        
        of file
        
         ezr32hg_gpio.h
        
        .
       
The documentation for this struct was generated from the following file:
- 
       C:/repos/embsw_super_h1/platform/Device/SiliconLabs/EZR32HG/Include/
       
ezr32hg_gpio.h