msdd.h File Reference
Mass Storage class Device (MSD) driver.
- Version
 - 5.4.0
 
License
Copyright 2015 Silicon Labs, Inc. http://www.silabs.com
This file is licensed under the Silabs License Agreement. See the file "Silabs_License_Agreement.txt" for details. Before using this software for any purpose, you must agree to the terms of that agreement.
       Definition in file
       
        msdd.h
       
       .
      
         Data Structures | 
       |
| struct | MSDD_CmdStatus_TypeDef | 
| 
         Status info for one BOT CBW -> Data I/O -> CSW cycle.
          | 
       |
         Macros | 
       |
| #define | MEDIA_BUFSIZ 4096 | 
         Functions | 
       |
| bool | MSDD_Handler (void) | 
| 
         Serve the MSD state machine. This function should be called on a regular basis from your main loop. It cannot be called from within an interrupt handler.
          | 
       |
| void | MSDD_Init (int activityLedPort, uint32_t activityLedPin) | 
| 
         Initialize MSD device.
          | 
       |
| int | MSDD_SetupCmd (const USB_Setup_TypeDef *setup) | 
| 
         Called whenever a USB setup command is received. This function overrides standard CLEAR_FEATURE commands, and implements MSD class commands "Bulk-Only Mass Storage Reset" and "Get Max LUN".
          | 
       |
| void | MSDD_StateChangeEvent ( USBD_State_TypeDef oldState, USBD_State_TypeDef newState) | 
| 
         Called whenever the USB device has changed its device state.
          | 
       |