textdisplay.h File Reference
Text display interface.
- Version
 - 5.4.0
 
License
Copyright 2015 Silicon Labs, Inc. http://www.silabs.com
This file is licensed under the Silabs License Agreement. See the file "Silabs_License_Agreement.txt" for details. Before using this software for any purpose, you must agree to the terms of that agreement.
       Definition in file
       
        textdisplay.h
       
       .
      
       #include <stdbool.h>
      
      
       #include "
       
        emstatus.h
       
       "
      
      
         Data Structures | 
       |
| struct | TEXTDISPLAY_Config_t | 
         Macros | 
       |
| #define | TEXTDISPLAY_EMSTATUS_ALREADY_INITIALIZED ( TEXTDISPLAY_EMSTATUS_BASE | 3) | 
| #define | TEXTDISPLAY_EMSTATUS_INVALID_PARAM ( TEXTDISPLAY_EMSTATUS_BASE | 1) | 
| #define | TEXTDISPLAY_EMSTATUS_NOT_ENOUGH_MEMORY ( TEXTDISPLAY_EMSTATUS_BASE | 5) | 
| #define | TEXTDISPLAY_EMSTATUS_NOT_INITIALIZED ( TEXTDISPLAY_EMSTATUS_BASE | 6) | 
| #define | TEXTDISPLAY_EMSTATUS_NOT_SUPPORTED ( TEXTDISPLAY_EMSTATUS_BASE | 4) | 
| #define | TEXTDISPLAY_EMSTATUS_OK (0) | 
| #define | TEXTDISPLAY_EMSTATUS_OUT_OF_RANGE ( TEXTDISPLAY_EMSTATUS_BASE | 2) | 
         Typedefs | 
       |
| typedef struct TEXTDISPLAY_Config_t | TEXTDISPLAY_Config_t | 
| typedef void * | TEXTDISPLAY_Handle_t | 
         Functions | 
       |
| EMSTATUS | TEXTDISPLAY_Delete ( TEXTDISPLAY_Handle_t handle) | 
| 
         Delete a text display device.
          | 
       |
| EMSTATUS | TEXTDISPLAY_LfToCrLf ( TEXTDISPLAY_Handle_t handle, bool on) | 
| 
         Enable or disable LF to CR+LF conversion.
          | 
       |
| EMSTATUS | TEXTDISPLAY_New ( TEXTDISPLAY_Config_t *config, TEXTDISPLAY_Handle_t *handle) | 
| 
         Create a new text display device.
          | 
       |
| EMSTATUS | TEXTDISPLAY_WriteChar ( TEXTDISPLAY_Handle_t handle, char c) | 
| 
         Write a single character to a text display.
          | 
       |
| EMSTATUS | TEXTDISPLAY_WriteString ( TEXTDISPLAY_Handle_t handle, const char *str) | 
| 
         Write a string of characters to a text display.
          | 
       |