emstatus.h File Reference
EMSTATUS definitions.
- Version
 - 5.5.0
 
License
Copyright 2015 Silicon Labs, Inc. http://www.silabs.com
This file is licensed under the Silabs License Agreement. See the file "Silabs_License_Agreement.txt" for details. Before using this software for any purpose, you must agree to the terms of that agreement.
       Definition in file
       
        emstatus.h
       
       .
      
       #include <stdint.h>
      
      
       #include "em_types.h"
      
      
         Macros | 
       |
| #define | DISPLAY_EMSTATUS_BASE (0x8011UL << 16) | 
| #define | EMSTATUS_OK (0) | 
| #define | PAL_EMSTATUS_BASE (0x8013UL << 16) | 
| #define | TEXTDISPLAY_EMSTATUS_BASE (0x8012UL << 16) | 
Macro Definition Documentation
| #define DISPLAY_EMSTATUS_BASE (0x8011UL << 16) | 
EMSTATUS base codes for display modules. EMSTATUS base code of DISPLAY driver interface.
        Definition at line
        
         26
        
        of file
        
         emstatus.h
        
        .
       
| #define EMSTATUS_OK (0) | 
Common EMSTATUS codes: Operation successful.
        Definition at line
        
         23
        
        of file
        
         emstatus.h
        
        .
       
| #define PAL_EMSTATUS_BASE (0x8013UL << 16) | 
EMSTATUS base code of PAL interface.
        Definition at line
        
         28
        
        of file
        
         emstatus.h
        
        .
       
| #define TEXTDISPLAY_EMSTATUS_BASE (0x8012UL << 16) | 
EMSTATUS base code of TEXTDISPLAY module.
        Definition at line
        
         27
        
        of file
        
         emstatus.h
        
        .