glib_line.c File Reference
Silicon Labs Graphics Library: Line Drawing Routines.
License
Copyright 2015 Silicon Labs, http://www.silabs.com
This file is licensensed under the Silabs License Agreement. See the file "Silabs_License_Agreement.txt" for details. Before using this software for any purpose, you must agree to the terms of that agreement.
       Definition in file
       
        glib_line.c
       
       .
      
       #include <stdint.h>
      
      
       #include <stdbool.h>
      
      
       #include "em_types.h"
      
      
       #include "
       
        glib.h
       
       "
      
      
         Functions | 
       |
| static bool | GLIB_clipLine ( GLIB_Context_t *pContext, int32_t *pX1, int32_t *pY1, int32_t *pX2, int32_t *pY2) | 
| 
         Clips the line if necessary, using the Cohen-Sutherland algorithm for clipping lines. See Wikipedia for algorithm.
          | 
       |
| EMSTATUS | GLIB_drawLine ( GLIB_Context_t *pContext, int32_t x1, int32_t y1, int32_t x2, int32_t y2) | 
| 
         Draws a line from x1,y1 to x2, y2.
          | 
       |
| EMSTATUS | GLIB_drawLineH ( GLIB_Context_t *pContext, int32_t x1, int32_t y1, int32_t x2) | 
| 
         Draws a horizontal line from x1, y1 to x2, y2.
          | 
       |
| EMSTATUS | GLIB_drawLineV ( GLIB_Context_t *pContext, int32_t x1, int32_t y1, int32_t y2) | 
| 
         Draws a vertical line from x1, y1 to x1, y2.
          | 
       |
| static uint8_t | GLIB_getClipCode ( GLIB_Context_t *pContext, int32_t x, int32_t y) | 
| 
         Gets the clip code for the point that is used by Cohen-Sutherland algorithm.
          | 
       |
Function Documentation
           
  | 
          static | 
Clips the line if necessary, using the Cohen-Sutherland algorithm for clipping lines. See Wikipedia for algorithm.
The points are moved using the linear equations: y=y0+slope*(x-x0),x=x0+(1/slope)*(y-y0)
- Parameters
 - 
         
pContextPointer to the GLIB_Context_t which holds the clipping region pX1Pointer to the start x-coordinate pY1Pointer to the start y-coordinate pX2Pointer to the end-x coordinate pY2Pointer to the end-y coordinate  
- Returns
 - Returns true if the line is inside, or crosses into, the clipping region, otherwise return false
 
        Definition at line
        
         244
        
        of file
        
         glib_line.c
        
        .
       
References __GLIB_Context_t::clippingRegion , GLIB_getClipCode() , __GLIB_Rectangle_t::xMax , __GLIB_Rectangle_t::xMin , __GLIB_Rectangle_t::yMax , and __GLIB_Rectangle_t::yMin .
Referenced by GLIB_drawLine() .
           
  | 
          static | 
Gets the clip code for the point that is used by Cohen-Sutherland algorithm.
- Parameters
 - 
         
pContextPointer to the GLIB_Context_t which holds the clipping region xStart x-coordinate yStart y-coordinate  
- Returns
 - Returns the 4-bit clip code
 
        Definition at line
        
         194
        
        of file
        
         glib_line.c
        
        .
       
References __GLIB_Context_t::clippingRegion , __GLIB_Rectangle_t::xMax , and __GLIB_Rectangle_t::yMax .
Referenced by GLIB_clipLine() .