tftdirect.c File Reference
EFM32GG_DK3750, TFT Initialization and setup for Direct Drive mode.
- Version
- 5.5.0
License
Copyright 2015 Silicon Labs, Inc. http://www.silabs.com
This file is licensed under the Silabs License Agreement. See the file "Silabs_License_Agreement.txt" for details. Before using this software for any purpose, you must agree to the terms of that agreement.
Definition in file tftdirect.c
.
#include <stdbool.h>
#include "em_device.h
"
#include "em_gpio.h
"
#include "em_ebi.h
"
#include "bsp.h
"
#include "tftdirect.h
"
#include "glib/glib.h
"
Functions | |
void | TFT_DirectGPIOConfig (void) |
GPIO configuration for TFT direct drive. | |
bool | TFT_DirectInit (const EBI_TFTInit_TypeDef *tftInit) |
TFT initialize or reinitialize Assumes EBI has been configured correctly in BSP_Init(BSP_INIT_DK_EBI) | |
Variables | |
static bool | runOnce = true |
Variable Documentation
|
static |
Flag to indicate that we need to initialize once if starting up in
Definition at line 26
of file tftdirect.c
.
Referenced by TFT_DirectInit().