touch.c File Reference
EFM32GG_DK3750, Touch panel driver.
- Version
 - 5.5.0
 
License
Copyright 2015 Silicon Labs, Inc. http://www.silabs.com
This file is licensed under the Silabs License Agreement. See the file "Silabs_License_Agreement.txt" for details. Before using this software for any purpose, you must agree to the terms of that agreement.
       Definition in file
       
        touch.c
       
       .
      
       #include <stdlib.h>
      
      
       #include <string.h>
      
      
       #include "
       
        em_device.h
       
       "
      
      
       #include "
       
        em_adc.h
       
       "
      
      
       #include "
       
        em_gpio.h
       
       "
      
      
       #include "
       
        em_cmu.h
       
       "
      
      
       #include "
       
        touch.h
       
       "
      
      
       #include "calibrate.h"
      
      
       #include "
       
        bsp.h
       
       "
      
      
       #include "
       
        i2cspm.h
       
       "
      
      
       #include "
       
        eeprom.h
       
       "
      
      
         Macros | 
       |
| #define | ADC_X adcSingleInpCh1 | 
| #define | ADC_Y adcSingleInpCh4 | 
| #define | TOUCH_X1_PIN 5 | 
| #define | TOUCH_X1_PORT gpioPortD | 
| #define | TOUCH_X2_PIN 4 | 
| #define | TOUCH_X2_PORT gpioPortD | 
| #define | TOUCH_Y1_PIN 3 | 
| #define | TOUCH_Y1_PORT gpioPortD | 
| #define | TOUCH_Y2_PIN 1 | 
| #define | TOUCH_Y2_PORT gpioPortD | 
         Enumerations | 
       |
| enum | 
         
          TOUCH_State_TypeDef
         
         {
          TOUCH_INIT , TOUCH_CHECK_PRESS , TOUCH_MEASURE_X , TOUCH_MEASURE_Y }  | 
       
         Functions | 
       |
| void | ADC0_IRQHandler (void) | 
| 
         Interrupt handler is executed with frequency ~28Hz when panel is not pressed and with frequency ~140Hz when panel is pressed - this will give ~50 readings per second.
          | 
       |
| int | TOUCH_CalibrationTable (POINT *displayPtr, POINT *screenPtr) | 
| 
         Set calibration table.
          | 
       |
| void | TOUCH_CallUpcall (void) | 
| 
         Function that calls registered upcall.
          | 
       |
| TOUCH_Pos_TypeDef * | TOUCH_GetPos (void) | 
| 
         Returns current touch position and state.
          | 
       |
| void | TOUCH_Init ( TOUCH_Config_TypeDef *config) | 
| 
         Initialize touch panel driver.
          | 
       |
| int | TOUCH_IsBusy (void) | 
| 
         Check status of the touch panel.
          | 
       |
| void | TOUCH_RecalculatePosition (volatile TOUCH_Pos_TypeDef *pos) | 
| 
         Convert ADC readings into XY position.
          | 
       |
| void | TOUCH_RegisterUpcall ( TOUCH_Upcall_TypeDef *new_upcall) | 
| 
         Register upcall which will be call every position or state change.
          | 
       |
| int | TOUCH_StateChanged (void) | 
| 
         Check if cursor state changed (down or move)
          | 
       |
         Variables | 
       |
| MATRIX | calibrationMatrix = { 103800, 2048, -8184704, -384, 102144, -16424640, 287650 } | 
Macro Definition Documentation
| #define ADC_X adcSingleInpCh1 | 
| #define ADC_Y adcSingleInpCh4 | 
Input channel 4
        Definition at line
        
         37
        
        of file
        
         touch.c
        
        .
       
Referenced by ADC0_IRQHandler() , and TOUCH_Init() .
| #define TOUCH_X1_PIN 5 | 
| #define TOUCH_X1_PORT gpioPortD | 
| #define TOUCH_X2_PIN 4 | 
Pin 4
        Definition at line
        
         43
        
        of file
        
         touch.c
        
        .
       
Referenced by ADC0_IRQHandler() , and TOUCH_IsBusy() .
| #define TOUCH_X2_PORT gpioPortD | 
Port D
        Definition at line
        
         42
        
        of file
        
         touch.c
        
        .
       
Referenced by ADC0_IRQHandler() , and TOUCH_IsBusy() .
| #define TOUCH_Y1_PIN 3 | 
| #define TOUCH_Y1_PORT gpioPortD | 
| #define TOUCH_Y2_PIN 1 | 
| #define TOUCH_Y2_PORT gpioPortD | 
Enumeration Type Documentation
| enum TOUCH_State_TypeDef | 
touch driver states
        Definition at line
        
         50
        
        of file
        
         touch.c
        
        .
       
Function Documentation
| void TOUCH_RecalculatePosition | ( | volatile TOUCH_Pos_TypeDef * | 
           
            pos
           
           | 
          ) | 
Convert ADC readings into XY position.
- Parameters
 - 
         
[in] posPointer to position structure  
        Definition at line
        
         158
        
        of file
        
         touch.c
        
        .
       
References TOUCH_Pos_TypeDef::adcx , TOUCH_Pos_TypeDef::adcy , calibrationMatrix , TOUCH_Pos_TypeDef::pen , TOUCH_Pos_TypeDef::x , and TOUCH_Pos_TypeDef::y .
Referenced by ADC0_IRQHandler() .
| int TOUCH_StateChanged | ( | void | 
           
           
           | 
          ) | 
Check if cursor state changed (down or move)
- Returns
 - 1 if the cursor state has changed
 
        Definition at line
        
         201
        
        of file
        
         touch.c
        
        .
       
References TOUCH_Pos_TypeDef::pen , TOUCH_Pos_TypeDef::x , and TOUCH_Pos_TypeDef::y .
Referenced by ADC0_IRQHandler() .
Variable Documentation
| MATRIX calibrationMatrix = { 103800, 2048, -8184704, -384, 102144, -16424640, 287650 } | 
Calibration table
        Definition at line
        
         70
        
        of file
        
         touch.c
        
        .
       
Referenced by TOUCH_CalibrationTable() , and TOUCH_RecalculatePosition() .