Structure representing characteristic service data.

This structure is used to define the parameters for characteristic service data, including the characteristic value property, handle, and UUID.

Public Attributes#

uint8_t

Characteristic value property.

uint8_t

Reserved.

uint16_t

Characteristic value handle.

Characteristic value attributes UUID.

Public Attribute Documentation#

char_property#

uint8_t char_serv_data_s::char_property

Characteristic value property.


Definition at line 605 of file components/device/silabs/si91x/wireless/ble/inc/rsi_ble_apis.h

reserved#

uint8_t char_serv_data_s::reserved

Reserved.


Definition at line 607 of file components/device/silabs/si91x/wireless/ble/inc/rsi_ble_apis.h

char_handle#

uint16_t char_serv_data_s::char_handle

Characteristic value handle.


Definition at line 609 of file components/device/silabs/si91x/wireless/ble/inc/rsi_ble_apis.h

char_uuid#

uuid_t char_serv_data_s::char_uuid

Characteristic value attributes UUID.


Definition at line 611 of file components/device/silabs/si91x/wireless/ble/inc/rsi_ble_apis.h