Structure representing the BLE request to set LE Long Term Key (LTK) request reply.
This structure is used to define the parameters for a BLE request to set the LE LTK request reply, including the address of the remote device, the type of reply (e.g., positive or negative), and the local Long Term Key (LTK).
Public Attributes#
uint8_t
Address of the remote device.
uint8_t
Type of reply (e.g., positive or negative)
uint8_t
Local Long Term Key (LTK) (16 bytes)
Public Attribute Documentation#
dev_addr#
uint8_t rsi_ble_set_le_ltkreqreply_s::dev_addr[RSI_DEV_ADDR_LEN]
Address of the remote device.
Definition at line
1160
of file components/device/silabs/si91x/wireless/ble/inc/rsi_ble.h
replytype#
uint8_t rsi_ble_set_le_ltkreqreply_s::replytype
Type of reply (e.g., positive or negative)
Definition at line
1162
of file components/device/silabs/si91x/wireless/ble/inc/rsi_ble.h
localltk#
uint8_t rsi_ble_set_le_ltkreqreply_s::localltk[16]
Local Long Term Key (LTK) (16 bytes)
Definition at line
1164
of file components/device/silabs/si91x/wireless/ble/inc/rsi_ble.h