Structure representing the BLE SMP (Security Manager Protocol) passkey.
This structure is used to define the parameters for a BLE SMP passkey, including the device address, reserved bytes for future use, and the passkey used for pairing.
Public Attributes#
uint8_t
Address of the device.
uint8_t
Reserved for future use (2 bytes)
uint32_t
Passkey used for pairing.
Public Attribute Documentation#
dev_addr#
uint8_t rsi_ble_smp_passkey_s::dev_addr[RSI_DEV_ADDR_LEN]
Address of the device.
Definition at line
843
of file components/device/silabs/si91x/wireless/ble/inc/rsi_ble.h
reserved#
uint8_t rsi_ble_smp_passkey_s::reserved[2]
Reserved for future use (2 bytes)
Definition at line
845
of file components/device/silabs/si91x/wireless/ble/inc/rsi_ble.h
passkey#
uint32_t rsi_ble_smp_passkey_s::passkey
Passkey used for pairing.
Definition at line
847
of file components/device/silabs/si91x/wireless/ble/inc/rsi_ble.h