Structure representing the BLE connection request.

This structure is used to define the parameters for a BLE connection request, including the address type and address of the device to connect, scan interval, scan window, connection interval, connection latency, and supervision timeout.

Public Attributes#

uint8_t

Address type of the device to connect.

uint8_t

Address of the device to connect.

uint16_t

Scan interval.

uint16_t

Scan window.

uint16_t

Minimum connection interval.

uint16_t

Maximum connection interval.

uint16_t

Connection latency.

uint16_t

Supervision timeout.

Public Attribute Documentation#

dev_addr_type#

uint8_t rsi_ble_req_conn_s::dev_addr_type

Address type of the device to connect.


dev_addr#

uint8_t rsi_ble_req_conn_s::dev_addr[RSI_DEV_ADDR_LEN]

Address of the device to connect.


le_scan_interval#

uint16_t rsi_ble_req_conn_s::le_scan_interval

Scan interval.


le_scan_window#

uint16_t rsi_ble_req_conn_s::le_scan_window

Scan window.


conn_interval_min#

uint16_t rsi_ble_req_conn_s::conn_interval_min

Minimum connection interval.


conn_interval_max#

uint16_t rsi_ble_req_conn_s::conn_interval_max

Maximum connection interval.


conn_latency#

uint16_t rsi_ble_req_conn_s::conn_latency

Connection latency.


supervision_tout#

uint16_t rsi_ble_req_conn_s::supervision_tout

Supervision timeout.