Structure representing the BLE command to set a long attribute value.
This structure is used to define the parameters for a BLE command to set a long attribute value, including the remote device address, the attribute handle, the attribute value offset, the length of the attribute value, and the attribute value itself.
Public Attributes#
uint8_t
Remote device address.
uint8_t
Attribute handle.
uint8_t
Attribute value offset.
uint8_t
Length of the attribute value.
uint8_t
Attribute value.
Public Attribute Documentation#
dev_addr#
uint8_t rsi_ble_set_long_att_val_s::dev_addr[RSI_DEV_ADDR_LEN]
Remote device address.
Definition at line
1409
of file components/device/silabs/si91x/wireless/ble/inc/rsi_ble.h
handle#
uint8_t rsi_ble_set_long_att_val_s::handle[2]
Attribute handle.
Definition at line
1411
of file components/device/silabs/si91x/wireless/ble/inc/rsi_ble.h
offset#
uint8_t rsi_ble_set_long_att_val_s::offset[2]
Attribute value offset.
Definition at line
1413
of file components/device/silabs/si91x/wireless/ble/inc/rsi_ble.h
length#
uint8_t rsi_ble_set_long_att_val_s::length
Length of the attribute value.
Definition at line
1415
of file components/device/silabs/si91x/wireless/ble/inc/rsi_ble.h
att_value#
uint8_t rsi_ble_set_long_att_val_s::att_value[RSI_DEV_ATT_LEN]
Attribute value.
Definition at line
1417
of file components/device/silabs/si91x/wireless/ble/inc/rsi_ble.h