Structure representing the BLE request for a long attribute value.
This structure is used to define the parameters for a BLE request to get a long attribute value, including the remote device address, the attribute handle, and the attribute value offset.
Public Attributes#
uint8_t
Remote device address.
uint16_t
Attribute handle.
uint16_t
Attribute value offset.
Public Attribute Documentation#
dev_addr#
uint8_t rsi_ble_req_long_att_value_s::dev_addr[RSI_DEV_ADDR_LEN]
Remote device address.
Definition at line
1348
of file components/device/silabs/si91x/wireless/ble/inc/rsi_ble.h
handle#
uint16_t rsi_ble_req_long_att_value_s::handle
Attribute handle.
Definition at line
1350
of file components/device/silabs/si91x/wireless/ble/inc/rsi_ble.h
offset#
uint16_t rsi_ble_req_long_att_value_s::offset
Attribute value offset.
Definition at line
1352
of file components/device/silabs/si91x/wireless/ble/inc/rsi_ble.h