Structure representing the BLE request for multiple attribute values.

This structure is used to define the parameters for a BLE request to get multiple attribute values, including the remote device address, the number of attribute handles, reserved bytes for future use, and the list of attribute handles.

Public Attributes#

uint8_t

Remote device address.

uint8_t

Number of attribute handles.

uint8_t

Reserved for future use.

uint16_t

List of attribute handles.

Public Attribute Documentation#

dev_addr#

uint8_t rsi_ble_req_multiple_att_val_s::dev_addr[RSI_DEV_ADDR_LEN]

Remote device address.


Definition at line 1326 of file components/device/silabs/si91x/wireless/ble/inc/rsi_ble.h

num_of_handles#

uint8_t rsi_ble_req_multiple_att_val_s::num_of_handles

Number of attribute handles.


Definition at line 1328 of file components/device/silabs/si91x/wireless/ble/inc/rsi_ble.h

reserved#

uint8_t rsi_ble_req_multiple_att_val_s::reserved

Reserved for future use.


Definition at line 1330 of file components/device/silabs/si91x/wireless/ble/inc/rsi_ble.h

handles#

uint16_t rsi_ble_req_multiple_att_val_s::handles[RSI_BLE_MAX_RESP_LIST]

List of attribute handles.


Definition at line 1332 of file components/device/silabs/si91x/wireless/ble/inc/rsi_ble.h