Structure representing the BLE Advertising Extensions (AE) command to set a random address.
This structure is used to define the parameters for a BLE AE command to set a random address, including the advertising handle and the random address.
Public Attributes#
uint8_t
Advertising_Handle, used to identify an advertising set, Range: 0x00 to 0xEF.
uint8_t
Random_Address, The Random Address may be of either Static Address or Private Address.
Public Attribute Documentation#
adv_handle#
uint8_t rsi_ble_ae_set_random_address_s::adv_handle
Advertising_Handle, used to identify an advertising set, Range: 0x00 to 0xEF.
Definition at line
1808
of file components/device/silabs/si91x/wireless/ble/inc/rsi_ble.h
addr#
uint8_t rsi_ble_ae_set_random_address_s::addr[RSI_DEV_ADDR_LEN]
Random_Address, The Random Address may be of either Static Address or Private Address.
Definition at line
1810
of file components/device/silabs/si91x/wireless/ble/inc/rsi_ble.h