Structure representing the BLE request to set an attribute value.
This structure is used to define the parameters for a BLE request to set an attribute value, including the remote device address, the attribute handle, the length of the attribute value, and the attribute value itself. The module will receive the acknowledgement from the remote device.
Public Attributes#
uint8_t
Remote device address.
uint8_t
Attribute handle.
uint8_t
Length of the attribute value.
uint8_t
Attribute value.
Public Attribute Documentation#
dev_addr#
uint8_t rsi_ble_set_att_val_s::dev_addr[RSI_DEV_ADDR_LEN]
Remote device address.
Definition at line
1370
of file components/device/silabs/si91x/wireless/ble/inc/rsi_ble.h
handle#
uint8_t rsi_ble_set_att_val_s::handle[2]
Attribute handle.
Definition at line
1372
of file components/device/silabs/si91x/wireless/ble/inc/rsi_ble.h
length#
uint8_t rsi_ble_set_att_val_s::length
Length of the attribute value.
Definition at line
1374
of file components/device/silabs/si91x/wireless/ble/inc/rsi_ble.h
att_value#
uint8_t rsi_ble_set_att_val_s::att_value[RSI_DEV_ATT_LEN]
Attribute value.
Definition at line
1376
of file components/device/silabs/si91x/wireless/ble/inc/rsi_ble.h