Structure representing the BLE request for profiles list.

This structure is used to define the parameters for a BLE request to get the profiles list, including the remote device address, the handle from which the profiles search will start, and the handle at which the profiles search will stop.

Public Attributes#

uint8_t

Remote device address.

uint16_t

Profiles search will start from this handle.

uint16_t

Profiles search will stop at this handle.

Public Attribute Documentation#

dev_addr#

uint8_t rsi_ble_req_profiles_list_s::dev_addr[RSI_DEV_ADDR_LEN]

Remote device address.


start_handle#

uint16_t rsi_ble_req_profiles_list_s::start_handle

Profiles search will start from this handle.


end_handle#

uint16_t rsi_ble_req_profiles_list_s::end_handle

Profiles search will stop at this handle.