Structure representing the BLE notification for an attribute value.
This structure is used to define the parameters for a BLE notification of an attribute value, including the remote device address, the attribute handle, the length of the attribute value, and the attribute value itself.
Public Attributes#
uint8_t
Remote device address.
uint16_t
Attribute handle.
uint16_t
Attribute value length.
uint8_t
Attribute value (data)
Public Attribute Documentation#
dev_addr#
uint8_t rsi_ble_notify_att_value_s::dev_addr[RSI_DEV_ADDR_LEN]
Remote device address.
Definition at line
1521
of file components/device/silabs/si91x/wireless/ble/inc/rsi_ble.h
handle#
uint16_t rsi_ble_notify_att_value_s::handle
Attribute handle.
Definition at line
1523
of file components/device/silabs/si91x/wireless/ble/inc/rsi_ble.h
data_len#
uint16_t rsi_ble_notify_att_value_s::data_len
Attribute value length.
Definition at line
1525
of file components/device/silabs/si91x/wireless/ble/inc/rsi_ble.h
data#
uint8_t rsi_ble_notify_att_value_s::data[RSI_DEV_ATT_LEN]
Attribute value (data)
Definition at line
1527
of file components/device/silabs/si91x/wireless/ble/inc/rsi_ble.h