Structure representing the parameters for writing RF path compensation values.

Public Attributes#

int16_t

int16_t, RF TX Path Compensation Value, Range: -128.0 dB (0xFB00) to 128.0 dB (0x0500)

int16_t

int16_t, RF RX Path Compensation Value, Range: -128.0 dB (0xFB00) to 128.0 dB (0x0500)

Public Attribute Documentation#

tx_path_value#

int16_t rsi_ble_write_rf_path_comp_s::tx_path_value

int16_t, RF TX Path Compensation Value, Range: -128.0 dB (0xFB00) to 128.0 dB (0x0500)


Definition at line 2342 of file components/device/silabs/si91x/wireless/ble/inc/rsi_ble.h

rx_path_value#

int16_t rsi_ble_write_rf_path_comp_s::rx_path_value

int16_t, RF RX Path Compensation Value, Range: -128.0 dB (0xFB00) to 128.0 dB (0x0500)


Definition at line 2344 of file components/device/silabs/si91x/wireless/ble/inc/rsi_ble.h