Structure representing the BLE command to update connection parameters.
This structure is used to define the parameters for a BLE command to update connection parameters, including the address of the connected device, minimum and maximum connection intervals, peripheral latency, and supervision timeout.
Public Attributes#
uint8_t
Address of the connected device.
uint16_t
Minimum connection interval.
uint16_t
Maximum connection interval.
uint16_t
Peripheral latency.
uint16_t
Supervision timeout.
Public Attribute Documentation#
dev_addr#
uint8_t rsi_ble_cmd_conn_params_update_s::dev_addr[RSI_DEV_ADDR_LEN]
Address of the connected device.
Definition at line
949
of file components/device/silabs/si91x/wireless/ble/inc/rsi_ble.h
min_interval#
uint16_t rsi_ble_cmd_conn_params_update_s::min_interval
Minimum connection interval.
Definition at line
951
of file components/device/silabs/si91x/wireless/ble/inc/rsi_ble.h
max_interval#
uint16_t rsi_ble_cmd_conn_params_update_s::max_interval
Maximum connection interval.
Definition at line
953
of file components/device/silabs/si91x/wireless/ble/inc/rsi_ble.h
latency#
uint16_t rsi_ble_cmd_conn_params_update_s::latency
Peripheral latency.
Definition at line
955
of file components/device/silabs/si91x/wireless/ble/inc/rsi_ble.h
timeout#
uint16_t rsi_ble_cmd_conn_params_update_s::timeout
Supervision timeout.
Definition at line
957
of file components/device/silabs/si91x/wireless/ble/inc/rsi_ble.h