Structure representing the BLE Credit Based Flow Control (CBFC) connection request.
This structure is used to define the parameters for a BLE CBFC connection request, including the address of the remote device and the Protocol/Service Multiplexer (PSM) value.
Public Attributes#
uint8_t
Address of the remote device.
uint8_t
Protocol/Service Multiplexer (PSM) value.
Public Attribute Documentation#
dev_addr#
uint8_t rsi_ble_cbfc_conn_req_s::dev_addr[RSI_DEV_ADDR_LEN]
Address of the remote device.
Definition at line
1042
of file components/device/silabs/si91x/wireless/ble/inc/rsi_ble.h
psm#
uint8_t rsi_ble_cbfc_conn_req_s::psm
Protocol/Service Multiplexer (PSM) value.
Definition at line
1044
of file components/device/silabs/si91x/wireless/ble/inc/rsi_ble.h