Structure representing a request to add an attribute in the BLE stack.
Public Attributes#
void *
service handler
uint16_t
Attribute handle.
uint16_t
If this variable is 1, Host has to maintain attributes and records in the application.
uint8_t
Attribute property.
uint16_t
Attribute data length.
uint8_t
Attribute data.
Public Attribute Documentation#
config_bitmap#
uint16_t rsi_ble_req_add_att_s::config_bitmap
If this variable is 1, Host has to maintain attributes and records in the application.
- If 0, Stack will maintain the attributes and records 
data#
uint8_t rsi_ble_req_add_att_s::data[RSI_DEV_ATT_LEN]
Attribute data.
The maximum value is 240, please refer RSI_DEV_ATT_LEN Macro