Structure representing the BLE GATT prepare write response.

This structure is used to define the parameters for a BLE GATT prepare write response, including the remote device address, the attribute handle, the attribute value offset, the length of the attribute value, and the attribute value itself.

Public Attributes#

uint8_t

Remote device address.

uint16_t

Attribute handle.

uint16_t

Attribute value offset.

uint16_t

Attribute value length.

uint8_t

Attribute value (data)

Public Attribute Documentation#

dev_addr#

uint8_t rsi_ble_gatt_prepare_write_response_s::dev_addr[RSI_DEV_ADDR_LEN]

Remote device address.


Definition at line 1619 of file components/device/silabs/si91x/wireless/ble/inc/rsi_ble.h

handle#

uint16_t rsi_ble_gatt_prepare_write_response_s::handle

Attribute handle.


Definition at line 1621 of file components/device/silabs/si91x/wireless/ble/inc/rsi_ble.h

offset#

uint16_t rsi_ble_gatt_prepare_write_response_s::offset

Attribute value offset.


Definition at line 1623 of file components/device/silabs/si91x/wireless/ble/inc/rsi_ble.h

data_len#

uint16_t rsi_ble_gatt_prepare_write_response_s::data_len

Attribute value length.


Definition at line 1625 of file components/device/silabs/si91x/wireless/ble/inc/rsi_ble.h

data#

uint8_t rsi_ble_gatt_prepare_write_response_s::data[RSI_DEV_ATT_LEN]

Attribute value (data)


Definition at line 1627 of file components/device/silabs/si91x/wireless/ble/inc/rsi_ble.h