tftamapped.c File Reference
EFM32GG_DK3750, TFT Initialization and setup for Adress Mapped mode.
- Version
 - 5.4.0
 
License
Copyright 2015 Silicon Labs, Inc. http://www.silabs.com
This file is licensed under the Silabs License Agreement. See the file "Silabs_License_Agreement.txt" for details. Before using this software for any purpose, you must agree to the terms of that agreement.
       Definition in file
       
        tftamapped.c
       
       .
      
       #include <stdbool.h>
      
      
       #include "
       
        em_device.h
       
       "
      
      
       #include "
       
        em_gpio.h
       
       "
      
      
       #include "
       
        em_ebi.h
       
       "
      
      
       #include "
       
        bsp.h
       
       "
      
      
       #include "
       
        tftamapped.h
       
       "
      
      
       #include "dmd/ssd2119/dmd_ssd2119.h"
      
      
       #include "
       
        glib/glib.h
       
       "
      
      
         Functions | 
       |
| bool | TFT_AddressMappedInit (void) | 
| 
         TFT initialize or reinitialize to Address Mapped Mode Assumes EBI has been configured correctly in BSP_Init(BSP_INIT_DK_EBI)
          | 
       |
         Variables | 
       |
| static bool | runOnce = true | 
Variable Documentation
           
  | 
          static | 
Flag to indicate that we need to initialize once if starting up in
        Definition at line
        
         27
        
        of file
        
         tftamapped.c
        
        .
       
Referenced by TFT_AddressMappedInit() .