displaypal.h File Reference
Platform Abstraction Layer (PAL) interface for DISPLAY driver.
- Version
 - 5.5.0
 
License
Copyright 2015 Silicon Labs, Inc. http://www.silabs.com
This file is licensed under the Silabs License Agreement. See the file "Silabs_License_Agreement.txt" for details. Before using this software for any purpose, you must agree to the terms of that agreement.
       Definition in file
       
        displaypal.h
       
       .
      
       #include "
       
        emstatus.h
       
       "
      
      
         Macros | 
       |
| #define | PAL_EMSTATUS_INVALID_PARAM ( PAL_EMSTATUS_BASE | 1) | 
| #define | PAL_EMSTATUS_OK (0) | 
| #define | PAL_EMSTATUS_REPEAT_FAILED ( PAL_EMSTATUS_BASE | 2) | 
Macro Definition Documentation
| #define PAL_EMSTATUS_INVALID_PARAM ( PAL_EMSTATUS_BASE | 1) | 
Invalid parameter.
        Definition at line
        
         31
        
        of file
        
         displaypal.h
        
        .
       
| #define PAL_EMSTATUS_OK (0) | 
EMSTATUS codes of the PAL interface. Operation successful.
        Definition at line
        
         30
        
        of file
        
         displaypal.h
        
        .
       
| #define PAL_EMSTATUS_REPEAT_FAILED ( PAL_EMSTATUS_BASE | 2) | 
Repeat failed.
        Definition at line
        
         32
        
        of file
        
         displaypal.h
        
        .