USTIMER
Detailed Description
USTIMER Microsecond Delay Timer Driver.
Implements microsecond delays.
The delay is implemented using a hardware timer. USTIMER_Init() must be called prior to using the delay functions. USTIMER_Init() must also be called if HFCORECLK and/or HFPERCLK is changed.
      The source files for the USTIMER driver library resides in the emdrv/ustimer folder, and are named
      
       ustimer.c
      
      and
      
       ustimer.h
      
      .
     
      
     
Introduction
The USTIMER driver implements microsecond delay functions. The delay is timed using a hardware TIMER or WTIMER resource. Two delay functions are available, one which uses energy mode EM1 to preserve energy while waiting, and one which performs busy wait.
- Note
 - Due to the overhead of setting up and serving TIMER/WTIMER interrupts, the USTIMER_Delay() function will be inaccurate for delays shorter than 200us. If higher accuracy is needed for short delays, consider using USTIMER_DelayIntSafe() or UDELAY_Delay() .
 
      
     
Configuration Options
By default the module use TIMER0. Timer resource selection is stored in a file named ustimer_config.h. A template for this file, containing default value, resides in the emdrv/config folder.
To configure USTIMER, provide your own configuration file. Here is a sample ustimer_config.h file:
      
     
The API
      This section contain brief descriptions of the functions in the API. You will find detailed information on input and output parameters and return values by clicking on the hyperlinked function names. Most functions return an error code,
      
       ECODE_EMDRV_USTIMER_OK
      
      is returned on success, see
      
       ecode.h
      
      and
      
       ustimer.h
      
      for other error codes.
     
      Your application code must include one header file:
      
       
        ustimer.h
       
      
      .
     
      
       USTIMER_Init()
      
      ,
      
       USTIMER_DeInit()
      
      
      These functions initialize and deinitialize the USTIMER driver. Typically USTIMER_Init() is called once in your startup code.
     
USTIMER_Delay() Delay a given number of microseconds. The MCU enters EM1 during the delay.
USTIMER_DelayIntSafe() Delay a given number of microseconds. The MCU stays in EM0 during the delay. This function can be called in any context and is also thread safe.
      
     
Example
         ustimer.h
        
        "
       
      
         Macros | 
       |
| #define | ECODE_EMDRV_USTIMER_OK ( ECODE_OK ) | 
| 
         Success return value.
          | 
       |
         Functions | 
       |
| Ecode_t | USTIMER_DeInit (void) | 
| 
         Deinitialize USTIMER driver.
          | 
       |
| Ecode_t | USTIMER_Delay (uint32_t usec) | 
| 
         Delay a given number of microseconds.
          | 
       |
| Ecode_t | USTIMER_DelayIntSafe (uint32_t usec) | 
| 
         Delay a given number of microseconds.
          | 
       |
| Ecode_t | USTIMER_Init (void) | 
| 
         Activate and initialize the hardware timer used to pace the 1 microsecond delay functions.
          | 
       |
Function Documentation
| Ecode_t USTIMER_DeInit | ( | void | 
           
           
           | 
          ) | 
Deinitialize USTIMER driver.
Will disable interrupts and turn off the clock to the underlying hardware timer.
- Returns
 - ECODE_EMDRV_USTIMER_OK .
 
        Definition at line
        
         220
        
        of file
        
         ustimer.c
        
        .
       
References CMU_ClockEnable() , ECODE_EMDRV_USTIMER_OK , TIMER_Enable() , TIMER_IntClear() , and TIMER_IntDisable() .
        Referenced by
        
         CAPT_enable()
        
        ,
        
         ezradio_comm_PollCTS()
        
        ,
        
         ezradio_reset()
        
        , and
        
         ezradioInit()
        
        .
       
| Ecode_t USTIMER_Delay | ( | uint32_t | 
           
            usec
           
           | 
          ) | 
Delay a given number of microseconds.
The mcu is put in EM1 during the delay.
- Note
 - This function assumes that the timer interrupt needed to wake the mcu up from EM1 is not blocked. This function is not thread safe. Due to the overhead of setting up and serving TIMER/WTIMER interrupts, timing will be inaccurate for delays shorter than 200us. If higher accuracy is needed for short delays, consider using USTIMER_DelayIntSafe() or UDELAY_Delay() .
 
- Parameters
 - 
         
[in] usecNumber of microseconds to delay.  
- Returns
 - ECODE_EMDRV_USTIMER_OK .
 
        Definition at line
        
         256
        
        of file
        
         ustimer.c
        
        .
       
References ECODE_EMDRV_USTIMER_OK .
Referenced by ezradio_comm_PollCTS() , ezradio_reset() , and ezradioInit() .
| Ecode_t USTIMER_DelayIntSafe | ( | uint32_t | 
           
            usec
           
           | 
          ) | 
Delay a given number of microseconds.
This is a busy wait delay not using energy modes to conserve power.
- Note
 - This function can be used in any context (interrupts can be disabled). This function is thread safe.
 
- Parameters
 - 
         
[in] usecNumber of microseconds to delay.  
- Returns
 - ECODE_EMDRV_USTIMER_OK .
 
        Definition at line
        
         290
        
        of file
        
         ustimer.c
        
        .
       
References ECODE_EMDRV_USTIMER_OK .
        Referenced by
        
         CAPT_enable()
        
        .
       
| Ecode_t USTIMER_Init | ( | void | 
           
           
           | 
          ) | 
Activate and initialize the hardware timer used to pace the 1 microsecond delay functions.
- Note
 - Call this function whenever the HFPERCLK and/or HFCORECLK frequency is changed.
 
- Returns
 - ECODE_EMDRV_USTIMER_OK .
 
        Definition at line
        
         154
        
        of file
        
         ustimer.c
        
        .
       
References CMU_ClockEnable() , CMU_ClockFreqGet() , cmuClock_CORE , cmuClock_HFPER , ECODE_EMDRV_USTIMER_OK , TIMER_InitCC_TypeDef::mode , TIMER_Init_TypeDef::prescale , TIMER_Init() , TIMER_INIT_DEFAULT , TIMER_InitCC() , TIMER_INITCC_DEFAULT , TIMER_IntDisable() , TIMER_TopSet() , timerCCModeCompare , and timerPrescale1024 .
        Referenced by
        
         CAPT_enable()
        
        ,
        
         ezradio_comm_PollCTS()
        
        ,
        
         ezradio_reset()
        
        , and
        
         ezradioInit()
        
        .