QSPI initialization structure.
       Definition at line
       
        187
       
       of file
       
        em_qspi.h
       
       .
      
      
       #include <
       
     
        em_qspi.h
       
       >
      
         Data Fields | 
       |
| uint8_t | divisor | 
| bool | enable | 
Field Documentation
| uint8_t QSPI_Init_TypeDef::divisor | 
Master mode baude rate divisor. Values can be even numbers in the range [2-32] inclusive.
        Definition at line
        
         194
        
        of file
        
         em_qspi.h
        
        .
       
Referenced by QSPI_Init() .
| bool QSPI_Init_TypeDef::enable | 
Enable/disable Quad SPI when initialization is completed.
        Definition at line
        
         189
        
        of file
        
         em_qspi.h
        
        .
       
Referenced by QSPI_Init() .
The documentation for this struct was generated from the following file:
- 
       C:/HandsOn/super/platform/emlib/inc/
       
em_qspi.h