CAN Message Object TypeDef structure. LSBs is used.
       Definition at line
       
        124
       
       of file
       
        em_can.h
       
       .
      
      
       #include <
       
     
        em_can.h
       
       >
      
         Data Fields | 
       |
| uint8_t | data [8] | 
| bool | directionMask | 
| uint8_t | dlc | 
| bool | extended | 
| bool | extendedMask | 
| uint32_t | id | 
| uint32_t | mask | 
| uint8_t | msgNum | 
Field Documentation
| uint8_t CAN_MessageObject_TypeDef::data[8] | 
A pointer to data, [0 - 8] bytes.
        Definition at line
        
         141
        
        of file
        
         em_can.h
        
        .
       
Referenced by CAN_ReadMessage() , and CAN_WriteData() .
| bool CAN_MessageObject_TypeDef::directionMask | 
Enable the use of 'direction' value for filtering.
        Definition at line
        
         150
        
        of file
        
         em_can.h
        
        .
       
Referenced by CAN_SetIdAndFilter() .
| uint8_t CAN_MessageObject_TypeDef::dlc | 
Data Length Code [0 - 8].
        Definition at line
        
         138
        
        of file
        
         em_can.h
        
        .
       
Referenced by CAN_ReadMessage() , CAN_SendMessage() , and CAN_WriteData() .
| bool CAN_MessageObject_TypeDef::extended | 
ID extended if true, standard if false.
        Definition at line
        
         129
        
        of file
        
         em_can.h
        
        .
       
Referenced by CAN_ReadMessage() , CAN_SendMessage() , and CAN_SetIdAndFilter() .
| bool CAN_MessageObject_TypeDef::extendedMask | 
Enable the use of 'extended' value for filtering.
        Definition at line
        
         147
        
        of file
        
         em_can.h
        
        .
       
Referenced by CAN_SetIdAndFilter() .
| uint32_t CAN_MessageObject_TypeDef::id | 
ID of the message with 11 bits (standard) or 28 bits (extended). LSBs are used for both.
        Definition at line
        
         135
        
        of file
        
         em_can.h
        
        .
       
Referenced by CAN_ReadMessage() , CAN_SendMessage() , and CAN_SetIdAndFilter() .
| uint32_t CAN_MessageObject_TypeDef::mask | 
A mask for ID filtering.
        Definition at line
        
         144
        
        of file
        
         em_can.h
        
        .
       
Referenced by CAN_SetIdAndFilter() .
| uint8_t CAN_MessageObject_TypeDef::msgNum | 
A message number of this Message Object, [1 - 32].
        Definition at line
        
         126
        
        of file
        
         em_can.h
        
        .
       
Referenced by CAN_ReadMessage() , CAN_SendMessage() , and CAN_SetIdAndFilter() .
The documentation for this struct was generated from the following file:
- 
       C:/HandsOn/super/platform/emlib/inc/
       
em_can.h