Backup Power Domain Initialization structure.
       Definition at line
       
        712
       
       of file
       
        em_emu.h
       
       .
      
      
       #include <
       
     
        em_emu.h
       
       >
      
         Data Fields | 
       |
| EMU_BUBuActPwrCon_TypeDef | activePwrCon | 
| bool | buVinProbeEn | 
| bool | disMaxComp | 
| bool | enable | 
| EMU_BUBuInactPwrCon_TypeDef | inactivePwrCon | 
| EMU_BUPwrRes_TypeDef | pwrRes | 
| bool | staEn | 
| EMU_BUVoutRes_TypeDef | voutRes | 
Field Documentation
| EMU_BUBuActPwrCon_TypeDef EMU_BUInit_TypeDef::activePwrCon | 
Power connection configuration when in backup mode.
        Definition at line
        
         715
        
        of file
        
         em_emu.h
        
        .
       
Referenced by EMU_BUInit() .
| bool EMU_BUInit_TypeDef::buVinProbeEn | 
| bool EMU_BUInit_TypeDef::disMaxComp | 
| bool EMU_BUInit_TypeDef::enable | 
| EMU_BUBuInactPwrCon_TypeDef EMU_BUInit_TypeDef::inactivePwrCon | 
Power connection configuration when not in backup mode.
        Definition at line
        
         714
        
        of file
        
         em_emu.h
        
        .
       
Referenced by EMU_BUInit() .
| EMU_BUPwrRes_TypeDef EMU_BUInit_TypeDef::pwrRes | 
| bool EMU_BUInit_TypeDef::staEn | 
Enable backup mode status export.
        Definition at line
        
         719
        
        of file
        
         em_emu.h
        
        .
       
Referenced by EMU_BUInit() .
| EMU_BUVoutRes_TypeDef EMU_BUInit_TypeDef::voutRes | 
The documentation for this struct was generated from the following file:
- 
       C:/HandsOn/super/platform/emlib/inc/
       
em_emu.h