LESENSE module initialization structure.
       Definition at line
       
        735
       
       of file
       
        em_lesense.h
       
       .
      
      
       #include <
       
     
        em_lesense.h
       
       >
      
         Data Fields | 
       |
| LESENSE_CoreCtrlDesc_TypeDef | coreCtrl | 
| LESENSE_DecCtrlDesc_TypeDef | decCtrl | 
| LESENSE_PerCtrlDesc_TypeDef | perCtrl | 
| LESENSE_TimeCtrlDesc_TypeDef | timeCtrl | 
Field Documentation
| LESENSE_CoreCtrlDesc_TypeDef LESENSE_Init_TypeDef::coreCtrl | 
LESENSE core configuration parameters.
        Definition at line
        
         737
        
        of file
        
         em_lesense.h
        
        .
       
Referenced by CAPLESENSE_setupLESENSE() , and LESENSE_Init() .
| LESENSE_DecCtrlDesc_TypeDef LESENSE_Init_TypeDef::decCtrl | 
LESENSE decoder configuration parameters.
        Definition at line
        
         746
        
        of file
        
         em_lesense.h
        
        .
       
Referenced by LESENSE_Init() .
| LESENSE_PerCtrlDesc_TypeDef LESENSE_Init_TypeDef::perCtrl | 
LESENSE peripheral configuration parameters.
        Definition at line
        
         743
        
        of file
        
         em_lesense.h
        
        .
       
Referenced by LESENSE_Init() .
| LESENSE_TimeCtrlDesc_TypeDef LESENSE_Init_TypeDef::timeCtrl | 
LESENSE timing configuration parameters.
        Definition at line
        
         740
        
        of file
        
         em_lesense.h
        
        .
       
Referenced by LESENSE_Init() .
The documentation for this struct was generated from the following file:
- 
       C:/HandsOn/super/platform/emlib/inc/
       
em_lesense.h